SABRE Board Analogue Video Input

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SABRE Board Analogue Video Input

ソリューションへジャンプ
2,617件の閲覧回数
samuelshort
Contributor I

Hi,


I wish to use the SABRE development board with the i.MX 6SoloX processor to develop computer vision processing and I require the use of the analogue video input on the processor. Does the SABRE board have access to this feature as I cannot find the 'video in' as an input to the board. The parallel camera connector is not sufficient as a key feature i require is compatibility with various cameras via an analogue video input.

Thank you,

Sam

ラベル(5)
0 件の賞賛
返信
1 解決策
2,502件の閲覧回数
Yuri
NXP Employee
NXP Employee

  VADC_IN signals are located on LCD expansion port. Please look at the schematic.


Have a great day,
YUri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,503件の閲覧回数
Yuri
NXP Employee
NXP Employee

  VADC_IN signals are located on LCD expansion port. Please look at the schematic.


Have a great day,
YUri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,502件の閲覧回数
samuelshort
Contributor I

Thank you Yuri,
Where can I find the schematic?

Kind Regards,
Sam

0 件の賞賛
返信
2,502件の閲覧回数
Yuri
NXP Employee
NXP Employee
0 件の賞賛
返信