Problem with kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with kernel

2,141 Views
marru
Contributor I

Hey, i get some problems with my Kernel.

In old Yocto the BUilding and baking worked fine.

 

Now i try to get the system into kirkstone. The Problem is, that i can all std-images, but not my own

 

I every get the same error:

 

NOTE: selecting linux-armour to satisfy runtime kernel-image due to PREFERRED_PROVIDER_virtual/kernel = linux-armour
DEBUG: sorted runtime providers for kernel-image are: ['/home/xxx/FP4_kirkstone/sources/meta-repl-armour/recipes-kernel/linux/linux-armour_4.1-2.0.x.bb']
DEBUG: adding '/home/xxx/FP4_kirkstone/sources/meta-repl-armour/recipes-kernel/linux/linux-armour_4.1-2.0.x.bb' to satisfy runtime 'kernel-image'
ERROR: Nothing RPROVIDES ''vmlinux',' (but /home/xxx/FP4_kirkstone/sources/meta-repl-armour/recipes-kernel/linux/linux-armour_4.1-2.0.x.bb RDEPENDS on or otherwise requires it)
NOTE: Runtime target ''vmlinux',' is unbuildable, removing...
Missing or unbuildable dependency chain was: ["'vmlinux',"]
DEBUG: File '/home/xxx/FP4_kirkstone/sources/meta-repl-armour/recipes-kernel/linux/linux-armour_4.1-2.0.x.bb' is unbuildable, removing...
NOTE: Target 'virtual/kernel' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['virtual/kernel', "'vmlinux',"]
DEBUG: File '/home/xxx/FP4_kirkstone/sources/meta-repl-armour/recipes-images/images/repl-flexi-panel-codesys.bb' is unbuildable, removing...
NOTE: Target 'repl-flexi-panel-codesys' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['repl-flexi-panel-codesys', 'virtual/kernel', "'vmlinux',"]
ERROR: Required build target 'repl-flexi-panel-codesys' has no buildable providers.
Missing or unbuildable dependency chain was: ['repl-flexi-panel-codesys', 'virtual/kernel', "'vmlinux',"]

 

What is my error, has anyone an advice to me?

 

Greetings

Marru

Labels (1)
0 Kudos
Reply
1 Reply

2,108 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

The latest yocto works with kernel 5.15.71, you are using 4.1., Those error are depency of the kernel Sorry it won't work. Try to download the yocto for dunfell or Zeus.

regards

 

0 Kudos
Reply