Problem with i.MX6UL Evk + LCD8000-43T + Buildroot Linux version 4.9.11.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with i.MX6UL Evk + LCD8000-43T + Buildroot Linux version 4.9.11.

2,944件の閲覧回数
igorlysenko
Contributor I

Hello All!

I use i.MX6UL Evk + LCD8000-43T.

 

If I load Yocto Linux, which was on microSD shipped with the EVK, everything is fine. First, i see on the LCD monitor a Uboot screen saver, then LInux Logo, then the Linux Graphical Shell.

Later I created an BuildRoot based Linux image - freescale_imx6ulevk_defconfig. But when it loading, on the LCD monitor  Uboot screen is displayed first, then LInux Logo and the blinking cursor and that's it. Further nothing changes and I do not see process of loading Linux on the LCD monitor.

I do not see an Linux Welcome after Linux is loaded on the LCD monitor. I can not enter commands from the keyboard.

 

But in the console I see that the Linux boot is proceeding normally.

 

My version of Linux does not have X11.

 

Note: via the console, I can display information on the monitor using the command
cat /dev/urandom > /dev/fb0

Igor.

ラベル(2)
2 返答(返信)

2,520件の閲覧回数
igorlysenko
Contributor I

Igor, Thanks for the answer!

But I need to try Buildroot.

Perhaps someone from the Embedded LInux Experts will tell me in which direction to look for the solution.

U-boot, .dtb or Linux Kernel configuration?

I do not see errors in the logs :smileysad: I do not know which direction to go in.

I attached log and config files.

Many thanks for the help.

============================================================

U-Boot

 

U-Boot 2017.03 (Mar 01 2018 - 23:10:09 +0200)

CPU:   Freescale i.MX6UL rev1.1 528 MHz (running at 396 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 35C
Reset cause: POR
Model: Freescale i.MX6 UltraLite 14x14 EVK Board
Board: MX6UL 14x14 EVK
DRAM:  512 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Display: TFT43AB (480x272)
Video: 480x272x24
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc1 is current device
Net:   eth1: ethernet@020b4000 [PRIME], eth0: ethernet@02188000
Normal Boot
Hit any key to stop autoboot:  0

=> print
baudrate=115200
board_name=EVK
board_rev=14X14
boot_fdt=try
bootcmd=run findfdt;mmc dev ${mmcdev};mmc dev ${mmcdev}; if mmc rescan; then if run loadbootscript; then run bootscript; else if run loadimage; then run mmcboot; else run netboot; fi; fi; else run netboot; fi
bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
bootdelay=3
bootscript=echo Running bootscript from mmc ...; source
console=ttymxc0
eth1addr=00:04:9f:04:ba:4d
ethact=ethernet@020b4000
ethaddr=00:04:9f:04:ba:4c
ethprime=eth1
fdt_addr=0x83000000
fdt_file=undefined
fdt_high=0xffffffff
fdtcontroladdr=9ef40f38
findfdt=if test $fdt_file = undefined; then if test $board_name = EVK && test $board_rev = 9X9; then setenv fdt_file imx6ul-9x9-evk.dtb; fi; if test $board_name = EVK && test $board_rev = 14X14; then setenv fdt_file imx6ul-14x14-evk.dtb; fi; if test $fdt_file = undefined; then echo WARNING: Could not determine dtb to use; fi; fi;
image=zImage
initrd_addr=0x83800000
initrd_high=0xffffffff
ip_dyn=yes
loadaddr=0x80800000
loadbootscript=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${script};
loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdt_file}
loadimage=fatload mmc ${mmcdev}:${mmcpart} ${loadaddr} ${image}
mfgtool_args=setenv bootargs console=${console},${baudrate} rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" clk_ignore_unused
mmcargs=setenv bootargs console=${console},${baudrate} root=${mmcroot}
mmcautodetect=yes
mmcboot=echo Booting from mmc ...; run mmcargs; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcdev=1
mmcpart=1
mmcroot=/dev/mmcblk1p2 rootwait rw
netargs=setenv bootargs console=${console},${baudrate} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
netboot=echo Booting from net ...; run netargs; if test ${ip_dyn} = yes; then setenv get_cmd dhcp; else setenv get_cmd tftp; fi; ${get_cmd} ${image}; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if ${get_cmd} ${fdt_addr} ${fdt_file}; then bootz ${loadaddr} - ${fdt_addr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
panel=TFT43AB
script=boot.scr

Environment size: 2526/8188 bytes

=================================================================

 

#dmesg

 

Booting Linux on physical CPU 0x0                                          
Linux version 4.9.11 (siddeveloper@Insp7559) (gcc version 6.4.0 (Buildroot 2018.02-rc1-00026-g7c384c3) ) #1 SMP PREEMPT Thu Mar 1 23:15:55 EET 2018
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c53c7d                                                                              
CPU: div instructions available: patching division code                   
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache                                                                     
OF: fdt:Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board                                                                                         
Reserved memory: created CMA memory pool at 0x8c000000, size 320 MiB
OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool                                                                  
Memory policy: Data cache writealloc                                   
On node 0 totalpages: 131072                                                                                                                 
free_area_init_node: node 0, pgdat 80f87680, node_mem_map 8bb57000                                           
 Normal zone: 1024 pages used for memmap                                  
 Normal zone: 0 pages reserved                                                                              
 Normal zone: 131072 pages, LIFO batch:31                                        
percpu: Embedded 14 pages/cpu @8bb31000 s25868 r8192 d23284 u57344         
pcpu-alloc: s25868 r8192 d23284 u57344 alloc=14*4096                                                                                                     
pcpu-alloc: [0] 0                                                                                                                            
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 130048                     
Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw
PID hash table entries: 2048 (order: 1, 8192 bytes)                                                          
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)                                                                                          
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory: 175880K/524288K available (9216K kernel code, 545K rwdata, 3208K rodata, 1024K init, 472K bss, 20728K reserved, 327680K cma-reserved, 0K highmem)
Virtual kernel memory layout:                                         
   vector  : 0xffff0000 - 0xffff1000   (   4 kB)                                                          
   fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)                                                                                            
   vmalloc : 0xa0800000 - 0xff800000   (1520 MB)                                                          
   lowmem  : 0x80000000 - 0xa0000000   ( 512 MB)                                                                                            
   pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)                                                                           
   modules : 0x7f000000 - 0x7fe00000   (  14 MB)                                                          
     .text : 0x80008000 - 0x80a00000   (10208 kB)                                                                                           
     .init : 0x80e00000 - 0x80f00000   (1024 kB)                                                                           
     .data : 0x80f00000 - 0x80f88460   ( 546 kB)                                                                                            
      .bss : 0x80f8a000 - 0x810003e0   ( 473 kB)                                                          
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1                               
Preemptible hierarchical RCU implementation.                                                               
       Build-time adjustment of leaf fanout to 32.                                                                                             
       RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.                                                 
RCU: Adjusting geometry for rcu_fanout_leaf=32, nr_cpu_ids=1                                                                                    
NR_IRQS:16 nr_irqs:16 16                                                                                                                     
Switching to timer-based delay loop, resolution 333ns                                                      
sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns                                                                   
clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns               
Console: colour dummy device 80x30                                                                                                              
Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)                                                     
pid_max: default: 32768 minimum: 301                                                                
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)                                                                                              
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)                                                                                         
CPU: Testing write buffer coherency: ok                                                                                                                  
/cpus/cpu@0 missing clock-frequency property                                                                                                             
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000                                                                                                         
Setting up static identity map for 0x80100000 - 0x80100058                                                                                   
Brought up 1 CPUs                                                                                                                                        
SMP: Total of 1 processors activated (6.00 BogoMIPS).                                                                                                    
CPU: All CPU(s) started in SVC mode.                                                                                                                     
devtmpfs: initialized                                                                                                                                    
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5                                                                                  
clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns                                                         
pinctrl core: initialized pinctrl subsystem                                                                                                  
NET: Registered protocol family 16                                                                  
DMA: preallocated 256 KiB pool for atomic coherent allocations                                      
cpuidle: using governor menu                                                                                 
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.                                                                              
hw-breakpoint: maximum watchpoint size is 8 bytes.                                                                                                       
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver                                                                                            
mxs-dma 1804000.dma-apbh: initialized                                                               
SCSI subsystem initialized                                                                                 
libata version 3.00 loaded.                                                                                                                  
usbcore: registered new interface driver usbfs                                                             
usbcore: registered new interface driver hub                                                                                                 
usbcore: registered new device driver usb                                                                                   
i2c i2c-0: IMX I2C adapter registered                                                                      
i2c i2c-0: can't use DMA, using PIO instead.                                                                                                 
i2c i2c-1: IMX I2C adapter registered                                                                                       
i2c i2c-1: can't use DMA, using PIO instead.                                                                                                 
Linux video capture interface: v2.00                                                                       
pps_core: LinuxPPS API ver. 1 registered                                                            
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <[email protected]>                   
PTP clock support registered                                                                                                                    
MIPI CSI2 driver module loaded                                                                               
imx rpmsg driver is registered.                                                                                                                 
Advanced Linux Sound Architecture Driver Initialized.                                                                                        
Bluetooth: Core ver 2.22                                                                                   
NET: Registered protocol family 31                                                                                                              
Bluetooth: HCI device and connection manager initialized                                                     
Bluetooth: HCI socket layer initialized    

Bluetooth: L2CAP socket layer initialized                                                           
Bluetooth: SCO socket layer initialized                                                                                                                  
clocksource: Switched to clocksource mxc_timer1                                                                                                          
VFS: Disk quotas dquot_6.6.0                                                                                                                             
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                                                                                          
NET: Registered protocol family 2                                                                                                                        
TCP established hash table entries: 4096 (order: 2, 16384 bytes)                                                                             
TCP bind hash table entries: 4096 (order: 3, 32768 bytes)                                                                                                
TCP: Hash tables configured (established 4096 bind 4096)                                                                                                 
UDP hash table entries: 256 (order: 1, 8192 bytes)                                                                                                       
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)                                                                                                  
NET: Registered protocol family 1                                                                                                                        
RPC: Registered named UNIX socket transport module.                                                                                                      
RPC: Registered udp transport module.                                                                                                        
RPC: Registered tcp transport module.                                                               
RPC: Registered tcp NFSv4.1 backchannel transport module.                                           
Bus freq driver module loaded                                                                                
futex hash table entries: 256 (order: 2, 16384 bytes)                                                                                                    
workingset: timestamp_bits=30 max_order=17 bucket_order=0                                                                                                
NFS: Registering the id_resolver key type                                                                                                                
Key type id_resolver registered                                                                     
Key type id_legacy registered                                                                              
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.                                                                                         
fuse init (API version 7.26)                                                                               
io scheduler noop registered                                                                                                                 
io scheduler deadline registered                                                                                            
io scheduler cfq registered (default)                                                                      
imx-weim 21b8000.weim: Driver registered.                                                                                                    
backlight supply power not found, using dummy regulator                                                                     
21c8000.lcdif supply lcd not found, using dummy regulator                                                                                    
mxsfb 21c8000.lcdif: failed to find mxc display driver                                                     
Console: switching to colour frame buffer device 60x34                                              
mxsfb 21c8000.lcdif: initialized                                                                           
imx-sdma 20ec000.sdma: loaded firmware 3.3                                                                                                      
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX                           
console [ttymxc0] enabled                                                                                                                       
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 66, base_baud = 5000000) is a IMX                                                           
imx sema4 driver is registered.                                                                            
[drm] Initialized                                                                                                                               
[drm] Initialized vivante 1.0.0 20120216 on minor 0          

brd: module loaded                                                                                                                                       
loop: module loaded                                                                                 
fsl-quadspi 21e0000.qspi: n25q256a (32768 Kbytes)                                                                                                        
spi_gpio spi4: gpio-miso property not found, switching to no-rx mode                                                                                     
libphy: Fixed MDIO Bus: probed                                                                                                                           
CAN device driver interface                                                                                                                              
flexcan 2090000.flexcan: device registered (reg_base=a099c000, irq=25)                                                                                   
flexcan 2094000.flexcan: device registered (reg_base=a09a4000, irq=26)                                                                       
20b4000.ethernet supply phy not found, using dummy regulator                                                                                             
pps pps0: new PPS source ptp0                                                                                                                            
libphy: fec_enet_mii_bus: probed                                                                                                                         
fec 20b4000.ethernet eth0: registered PHC device 0                                                                                                       
2188000.ethernet supply phy not found, using dummy regulator                                                                                             
pps pps1: new PPS source ptp1                                                                                                                            
fec 2188000.ethernet eth1: registered PHC device 1                                                                                           
usbcore: registered new interface driver kaweth                                                     
pegasus: v0.9.3 (2013/04/25), Pegasus/Pegasus II USB Ethernet driver                                
usbcore: registered new interface driver pegasus                                                             
usbcore: registered new interface driver rtl8150                                                                                                         
usbcore: registered new interface driver r8152                                                                                                           
usbcore: registered new interface driver asix                                                                                                            
usbcore: registered new interface driver ax88179_178a                                               
usbcore: registered new interface driver cdc_ether                                                         
usbcore: registered new interface driver net1080                                                                                             
usbcore: registered new interface driver cdc_subset                                                        
usbcore: registered new interface driver zaurus                                                                                              
usbcore: registered new interface driver cdc_ncm                                                                            
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver                                                 
ehci-mxc: Freescale On-Chip EHCI Host driver                                                                                                 
usbcore: registered new interface driver usb-storage                                                                        
usbcore: registered new interface driver usb_ehset_test                                                                                      
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator                                        
2184000.usb supply vbus not found, using dummy regulator                                            
2184200.usb supply vbus not found, using dummy regulator                                                   
ci_hdrc ci_hdrc.1: EHCI Host Controller                                                                                                         
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 1                                             
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00                                                                                                   
hub 1-0:1.0: USB hub found                                                                                                                   
hub 1-0:1.0: 1 port detected                                                                               
mousedev: PS/2 mouse device common for all mice                                                                                                 
input: 20cc000.snvs:snvs-powerkey as /devices/soc0/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
input: iMX6UL Touchscreen Controller as /devices/soc0/soc/2000000.aips-bus/2040000.tsc/input/input1    

input: FreescaleAccelerometer as /devices/virtual/input/input2                                                                                           
fxls8471 device driver probe successfully                                                                                                                
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0                                                                      
i2c /dev entries driver                                                                                                                                  
IR NEC protocol handler initialized                                                                                                                      
IR RC5(x/sz) protocol handler initialized                                                                                                    
IR RC6 protocol handler initialized                                                                                                                      
IR JVC protocol handler initialized                                                                                                                      
IR Sony protocol handler initialized                                                                                                                     
IR SANYO protocol handler initialized                                                                                                                    
IR Sharp protocol handler initialized                                                                                                                    
IR MCE Keyboard/mouse protocol handler initialized                                                                                                       
IR XMP protocol handler initialized                                                                                                          
pxp-v4l2 pxp_v4l2: initialized                                                                                              
0-000e supply vdd not found, using dummy regulator                                                                          
0-000e supply vddio not found, using dummy regulator                                                                        
mag3110 0-000e: check mag3110 chip ID                                                                                                                    
input: mag3110 as /devices/virtual/input/input3                                                                                                          
random: fast init done                                                                                                                                   
mag3110 0-000e: mag3110 is probed                                                                                           
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)                                                                          
Bluetooth: HCI UART driver ver 2.3                                                                                                           
Bluetooth: HCI UART protocol H4 registered                                                                                  
Bluetooth: HCI UART protocol BCSP registered                                                                                                 
Bluetooth: HCI UART protocol ATH3K registered                                                                               
usbcore: registered new interface driver bcm203x                                                                            
usbcore: registered new interface driver btusb                                                                                               
usbcore: registered new interface driver ath3k                                                                              
sdhci: Secure Digital Host Controller Interface driver                                                                                       
sdhci: Copyright(c) Pierre Ossman                                                                                           
sdhci-pltfm: SDHCI platform and OF driver helper                                                                            
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO                                                                                  
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA                                                                              
sdhci-esdhc-imx 2194000.usdhc: could not get ultra high speed state, work on normal mode                                    
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA                                                                              
usb 1-1: new high-speed USB device number 2 using ci_hdrc                                                                                    
caam 2140000.caam: ERA source: CCBVID.                                                                                      
caam 2140000.caam: Entropy delay = 3200                                                                                                         
caam 2140000.caam: Instantiated RNG4 SH0                                                                                    
mmc1: host does not support reading read-only switch, assuming write-enable                          

mmc1: new high speed SDHC card at address 1234                                                                                                           
caam 2140000.caam: Instantiated RNG4 SH1                                                                                                                 
caam 2140000.caam: device ID = 0x0a16030000000000 (Era 8)                                                                   
caam 2140000.caam: job rings = 3, qi = 0                                                                                                                 
mmcblk1: mmc1:1234 SA04G 3.68 GiB                                                                                                                        
mmcblk1: p1 p2                                                                                                                                          
hub 1-1:1.0: USB hub found                                                                                                                               
hub 1-1:1.0: 4 ports detected                                                                                                                            
caam algorithms registered in /proc/crypto                                                                                                   
caam_jr 2141000.jr0: registering rng-caam                                                                                                                
caam 2140000.caam: caam pkc algorithms registered in /proc/crypto                                                                                        
platform caam_sm: blkkey_ex: 8 keystore units available                                                                                                  
platform caam_sm: 64-bit clear key:                                                                                                                      
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07                                                                                                         
platform caam_sm: 64-bit black key:                                                                                                                      
platform caam_sm: [0000] 93 8f 4b 00 53 dd 86 d4                                                                                             
platform caam_sm: [0008] d6 8b 20 f0 88 63 c5 8e                                                                            
platform caam_sm: 128-bit clear key:                                                                                        
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07                                                                            
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f                                                                                                         
platform caam_sm: 128-bit black key:                                                                                                                     
platform caam_sm: [0000] c8 f1 fc 56 12 4d 6d cd                                                                                                         
platform caam_sm: [0008] 39 1e 16 eb d7 03 df 12                                                                            
platform caam_sm: 192-bit clear key:                                                                                        
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07                                                                                             
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f                                                                            
platform caam_sm: [0016] 10 11 12 13 14 15 16 17                                                                                             
platform caam_sm: 192-bit black key:                                                                                        
platform caam_sm: [0000] 8a b0 ad e2 87 5a 5c 8b                                                                            
platform caam_sm: [0008] 86 e1 97 92 3c 47 69 7a                                                                                             
platform caam_sm: [0016] b0 71 b7 45 0b 32 b8 5d                                                                            
platform caam_sm: [0024] 49 da 45 62 72 d9 cc 72                                                                                             
platform caam_sm: 256-bit clear key:                                                                                        
platform caam_sm: [0000] 00 01 02 03 04 0f 06 07                                                                            
platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f                                                                            
platform caam_sm: [0016] 10 11 12 13 14 15 16 17                                                                                                
platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f                                                                            
platform caam_sm: 256-bit black key:                                                                                                            
platform caam_sm: [0000] 20 e4 b4 16 84 64 2e 9e                                                                                             
platform caam_sm: [0008] 97 01 5c 1d 2b f1 40 87                                                                            
platform caam_sm: [0016] d5 a5 72 48 de d2 64 3e                                                                                                
platform caam_sm: [0024] 2c e4 82 fa 62 dd 1d 44                                                                            
platform caam_sm: 64-bit unwritten blob:                                     

platform caam_sm: 64-bit unwritten blob:                                                                                                                 
platform caam_sm: [0000] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0008] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0016] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0024] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0032] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0040] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0048] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0056] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: 128-bit unwritten blob:                                                                                                                
platform caam_sm: [0000] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0008] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0016] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0024] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0032] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0040] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0048] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0056] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: 196-bit unwritten blob:                                                                                   
platform caam_sm: [0000] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0008] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0016] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0024] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0032] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0040] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0048] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0056] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                                                
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                                                
platform caam_sm: 256-bit unwritten blob:        

platform caam_sm: [0000] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0008] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0016] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0024] 00 00 00 00 00 00 00 00                                                                                                         
usb 1-1.2: new high-speed USB device number 3 using ci_hdrc                                                                                              
platform caam_sm: [0032] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0040] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0048] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0056] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: 64-bit black key in blob:                                                                                                              
platform caam_sm: [0000] 12 b9 09 e3 46 20 52 5b                                                                                                         
platform caam_sm: [0008] ed 73 e6 d4 23 59 db d0                                                                                             
platform caam_sm: [0016] 01 ed 0a 7f f6 64 ae c4                                                                            
platform caam_sm: [0024] 5e 66 a0 42 e5 e8 2f d4                                                                            
platform caam_sm: [0032] 9d ae 5e ff 82 9d 62 bb                                                                            
platform caam_sm: [0040] 68 ab 12 5b 66 80 8e 32                                                                                                         
platform caam_sm: [0048] f9 cf 64 db 3c 86 91 3f                                                                                                         
platform caam_sm: [0056] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: 128-bit black key in blob:                                                                                                 
platform caam_sm: [0000] ff bf 3f e1 49 cf 53 d6                                                                            
platform caam_sm: [0008] af ab 8e cb 8b 63 81 3e                                                                            
platform caam_sm: [0016] dd 09 6a d6 87 58 c5 b2                                                                                             
platform caam_sm: [0024] b9 9c 36 a2 43 fa b1 db                                                                            
platform caam_sm: [0032] 2e 89 4f bc c8 f7 a8 43                                                                                             
platform caam_sm: [0040] d5 db 0f 96 fc ef c2 94                                                                            
platform caam_sm: [0048] 71 1a 9b 81 9b 2c 7e 61                                                                            
platform caam_sm: [0056] ef c5 80 48 96 be 27 ae                                                                            
platform caam_sm: [0064] 00 00 00 00 00 00 00 00                                                                                                
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                                
platform caam_sm: [0088] 00 00 00 00 00 00 00 00        

 

platform caam_sm: 192-bit black key in blob:                                                                                                             
platform caam_sm: [0000] 25 52 2d 7d 47 bd 21 08                                                                                                         
platform caam_sm: [0008] 32 06 48 08 f1 e8 87 47                                                                            
platform caam_sm: [0016] 37 5f a8 da 70 f2 59 ac                                                                                                         
platform caam_sm: [0024] de 8d 95 64 1a e8 85 cb                                                                                                         
platform caam_sm: [0032] ef 3b df c4 bc aa 92 fb                                                                                                         
platform caam_sm: [0040] 9a 43 aa 8c 37 61 9d da                                                                                                         
platform caam_sm: [0048] 68 e6 35 3e fe af a0 da                                                                                                         
platform caam_sm: [0056] d7 4a 45 d8 30 d7 74 9c                                                                                             
platform caam_sm: [0064] 50 65 13 6e eb a1 57 9d                                                                                                         
platform caam_sm: [0072] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                                                         
platform caam_sm: 256-bit black key in blob:                                                                                                             
platform caam_sm: [0000] 3a 42 d5 bf e0 c4 27 40                                                                                                         
platform caam_sm: [0008] 69 6f bc 4a ba 3f ae 1e                                                                                             
platform caam_sm: [0016] 02 a1 f9 07 48 d1 c9 b6                                                                            
platform caam_sm: [0024] d4 1c ff 8a a8 01 7a 0a                                                                            
platform caam_sm: [0032] 4e 54 2d 10 21 3b ac c9                                                                            
platform caam_sm: [0040] e5 f5 77 1a da 6f 70 87                                                                                                         
platform caam_sm: [0048] 94 ea a5 5a 4a 14 11 71                                                                                                         
platform caam_sm: [0056] d6 77 ec 72 c3 7f e0 18                                                                                                         
platform caam_sm: [0064] e4 c0 93 a8 72 9c b9 8a                                                                            
platform caam_sm: [0072] 1d 8c 70 40 7a 21 c0 46                                                                            
platform caam_sm: [0080] 00 00 00 00 00 00 00 00                                                                                             
platform caam_sm: [0088] 00 00 00 00 00 00 00 00                                                                            
platform caam_sm: restored 64-bit black key:                                                                                                 
platform caam_sm: [0000] 8c 3a e6 e7 c2 0a f6 7f                                                                            
platform caam_sm: [0008] f3 b5 48 35 c3 3d b3 d6                                                                            
platform caam_sm: restored 128-bit black key:                                                                                                
platform caam_sm: [0000] c8 f1 fc 56 12 4d 6d cd                                                                            
platform caam_sm: [0008] 39 1e 16 eb d7 03 df 12                                                                                             
platform caam_sm: restored 192-bit black key:                                                                               
platform caam_sm: [0000] 8a b0 ad e2 87 5a 5c 8b                                                                            
platform caam_sm: [0008] 86 e1 97 92 3c 47 69 7a                                                                            
platform caam_sm: [0016] 08 f3 28 11 c6 b0 70 c6                    

usb 1-1.3: new low-speed USB device number 4 using ci_hdrc                                                                                               
platform caam_sm: [0024] a0 61 c3 31 68 df 40 49                                                                                                         
platform caam_sm: restored 256-bit black key:                                                                               
platform caam_sm: [0000] 20 e4 b4 16 84 64 2e 9e                                                                                                         
platform caam_sm: [0008] 97 01 5c 1d 2b f1 40 87                                                                                                         
platform caam_sm: [0016] d5 a5 72 48 de d2 64 3e                                                                                                         
platform caam_sm: [0024] 2c e4 82 fa 62 dd 1d 44                                                                                                         
snvs-secvio 20cc000.caam-snvs: can't get snvs clock                                                                                                      
snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state                                                                   
usbcore: registered new interface driver usbhid                                                                                                          
usbhid: USB HID core driver                                                                                                                              
imx-wm8960 sound: wm8960-hifi <-> 202c000.sai mapping ok                                                                                                 
imx-wm8960 sound: snd-soc-dummy-dai <-> 2034000.asrc mapping ok                                                                                          
imx-wm8960 sound: wm8960-hifi <-> 202c000.sai mapping ok                                                                                                 
input: USB USB Keyboard as /devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.3/1-1.3:1.0/0003:1A2C:2C27.0001/input/input4            
NET: Registered protocol family 26                                                                                                           
NET: Registered protocol family 10                                                                                          
hid-generic 0003:1A2C:2C27.0001: input: USB HID v1.10 Keyboard [USB USB Keyboard] on usb-ci_hdrc.1-1.3/input0                                
sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver                                                                                          
NET: Registered protocol family 17                                                                                                                       
can: controller area network core (rev 20120528 abi 9)                                                                                                   
NET: Registered protocol family 29                                                                                                                       
can: raw protocol (rev 20120528)                                                                                                             
can: broadcast manager protocol (rev 20161123 t)                                                                                             
can: netlink gateway (rev 20130117) max_hops=1                                                                                               
Bluetooth: RFCOMM TTY layer initialized                                                                                                      
Bluetooth: RFCOMM socket layer initialized                                                                                                   
Bluetooth: RFCOMM ver 1.11                                                                                                                   
Bluetooth: BNEP (Ethernet Emulation) ver 1.3                                                                                                 
Bluetooth: BNEP filters: protocol multicast                                                                                                  
Bluetooth: BNEP socket layer initialized                                                                                                     
Bluetooth: HIDP (Human Interface Emulation) ver 1.2                                                                                          
Bluetooth: HIDP socket layer initialized                                                                                                     
8021q: 802.1Q VLAN Support v1.8                                                                                             
Key type dns_resolver registered                                                                                            
cpu cpu0: Registered imx6q-cpufreq                                                                                                              
imx_thermal 2000000.aips-bus:tempmon: Industrial CPU temperature grade - max:105C critical:100C passive:95C                 
input: USB USB Keyboard as /devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.3/1-1.3:1.1/0003:1A2C:2C27.0002/input/input6   
dhd_module_init in                                                                                                                           
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:57:59 UTC (3479)                                   
VSD_3V3: disabling                                                                                                                              
can-3v3: disabling                                                                                                                           
gpio_dvfs: disabling                  

ALSA device list:                                                                                                                            
 #0: wm8960-audio                                                                                                                           
hid-generic 0003:1A2C:2C27.0002: input: USB HID v1.10 Device [USB USB Keyboard] on usb-ci_hdrc.1-1.3/input1                                  
EXT4-fs (mmcblk1p2): couldn't mount as ext3 due to feature incompatibilities                                                
usb 1-1.1: new low-speed USB device number 5 using ci_hdrc                                                                  
input: 2.4G Wireless Mouse as /devices/soc0/soc/2100000.aips-bus/2184200.usb/ci_hdrc.1/usb1/1-1/1-1.1/1-1.1:1.0/0003:04F3:02F4.0003/input/input7
hid-generic 0003:04F3:02F4.0003: input: USB HID v1.11 Mouse [2.4G Wireless Mouse] on usb-ci_hdrc.1-1.1/input0               
EXT4-fs (mmcblk1p2): recovery complete                                                                                                          
EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null)                                                                    
VFS: Mounted root (ext4 filesystem) on device 179:18.                                                                       
devtmpfs: mounted                                                                                                                               
Freeing unused kernel memory: 1024K (80e00000 - 80f00000)                                                                                    
EXT4-fs (mmcblk1p2): re-mounted. Opts: data=ordered   

 

==========================================================

0 件の賞賛
返信

2,520件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Igor

one can try to build image using nxp documentation on

i.MX Software|NXP 

Buildroot is not supported by nxp, one can look on boundary devices

guidelines:

Buildroot Getting Started Guide - Boundary Devices 

Buildroot - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------