Problem with PMIC GAUX signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with PMIC GAUX signal

1,381 Views
AhmedShameemM_1
Contributor I

Hello,

 I am using MC34708 PMIC for i.MX 50 QS Board, and there is a problem in GAUX signal of PMIC. GAUX is supposed to be low when we give power supply,but in one of my board it becomes high after 12sec.Can any one help me to solve this problem. Waiting for reply......

Regards

Ahmed Shameem

0 Kudos
Reply
1 Reply

1,347 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Ahmed,

 

Gaux will enable Maux when the USB charger is disconnected and Vaux is valid. It will disable Maux in case of a low voltage or over voltage condition, or if the USB charger is present. What voltage do you see at VBUS and VAUX when the issue occurs?

 

Best regards.

Jorge.

0 Kudos
Reply