Problem while start Android5.0 on i.mx6, showing "binder: 135:135 transaction failed 29189, size 0-0"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem while start Android5.0 on i.mx6, showing "binder: 135:135 transaction failed 29189, size 0-0"

2,959 Views
gushi
Contributor I

Pls help.

     I'have got all the source code from freescale website and followed the instructs of "Android_Quick_Start_Guide.pdf".

 

while all have down;

 

then i copy these files to mfgtools's files directory. "mfgtool\IMX-L5.0.0-MFG-TOOL\Profiles\Linux\OS Firmware\files\android\"

These are the name of 4 files, while copy to mfgtools .

boot-imx6q.img

recovery-imx6q.img

system.img

u-boot-imx6q.imx

 

writing progress turns be all OK, the i change boot config sw to '01000010', boot from Sabresd-SDB board.

after about 30 seconds, then continuing show "binder: 135:135 transaction failed 29189, size 0-0", then reboot after some time.

 

what's the problem???

 

some of the booting log shows below ...

 

....

Bluetooth: RFCOMM TTY layer initialized

Bluetooth: RFCOMM socket layer initialized

Bluetooth: RFCOMM ver 1.11

Bluetooth: BNEP (Ethernet Emulation) ver 1.3

Bluetooth: BNEP filters: protocol multicast

Bluetooth: BNEP socket layer initialized

Bluetooth: HIDP (Human Interface Emulation) ver 1.2

Bluetooth: HIDP socket layer initialized

8021q: 802.1Q VLAN Support v1.8

Key type dns_resolver registered

VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4

VGEN1: disabling

SWBST: disabling

SW4: disabling

wm8962-supply: disabling

usb_otg_vbus: disabling

regulator-dummy: disabling

imx mcc test is registered.

file system registered

android_usb gadget: Mass Storage Function, version: 2009/09/11

android_usb gadget: Number of LUNs=1

lun0: LUN: removable file: (no medium)

android_usb gadget: android_usb ready

input: gpio-keys.27 as /devices/soc0/gpio-keys.27/input/input5

snvs_rtc 20cc034.snvs-rtc-lp: setting system clock to 1970-01-01 00:00:40 UTC (40)

ALSA device list:

  #0: wm8962-audio

  #1: imx-hdmi-soc

Freeing unused kernel memory: 340K (80e7b000 - 80ed0000)

type=1403 audit(40.710:2): policy loaded auid=4294967295 ses=4294967295

type=1404 audit(40.720:3): enforcing=1 old_enforcing=0 auid=4294967295 ses=4294967295

init: /dev/hw_random not found

Console: switching to colour dummy device 80x30

init: /dev/hw_random not found

fs_mgr: Could not open block device /dev/block/mmcblk3p5 (No such file or directory).

fs_mgr: Could not set up verified partition, skipping!

fs_mgr: __mount(source=/dev/block/mmcblk3p4,target=/data,type=ext4)=-1

fs_mgr: fs_mgr_mount_all(): possibly an encryptable blkdev /dev/block/mmcblk3p4 for mount /data type ext4 )

fs_mgr: __mount(source=/dev/block/mmcblk3p6,target=/cache,type=ext4)=-1

fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p6 at /cache options: nomblk_io_submit error: No such file or directory

fs_mgr: __mount(source=/dev/block/mmcblk3p7,target=/device,type=ext4)=-1

fs_mgr: Failed to mount an un-encryptable or wiped partition on/dev/block/mmcblk3p7 at /device options: (null) error: No such file or directory

init: fs_mgr_mount_all returned an error

init: fs_mgr_mount_all returned unexpected error 255

SELinux: Could not set context for /cache:  Read-only file system

rfkill: BT RF going to : off

init: cannot find '/system/bin/logd', disabling 'logd'

init: cannot find '/system/bin/lmkd', disabling 'lmkd'

binder: 135:135 transaction failed 29189, size 0-0

init: cannot find '/system/bin/servicemanager', disabling 'servicemanager'

init: cannot find '/system/bin/vold', disabling 'vold'

init: cannot find '/system/bin/surfaceflinger', disabling 'surfaceflinger'

init: using deprecated syntax for specifying property 'ro.serialno', use ${name} instead

init: property 'ro.serialno' doesn't exist while expanding '$ro.serialno'

init: cannot expand '$ro.serialno' while writing to '/sys/class/android_usb/android0/iSerial'

init: using deprecated syntax for specifying property 'ro.product.manufacturer', use ${name} instead

init: property 'ro.product.manufacturer' doesn't exist while expanding '$ro.product.manufacturer'

init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufacturer'

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'

init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'

android_usb: already disabled

mtp_bind_config

android_work: sent uevent USB_STATE=CONNECTED

android_work: sent uevent USB_STATE=DISCONNECTED

android_work: sent uevent USB_STATE=CONNECTED

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

android_usb gadget: high-speed config #1: android

android_work: sent uevent USB_STATE=CONFIGURED

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

binder: 135:135 transaction failed 29189, size 0-0

Original Attachment has been moved to: session.log.zip

Labels (4)
0 Kudos
Reply
2 Replies

1,565 Views
chandrasekharma
Contributor III

Hi....

I am getting same issue regarding booting of android - 5.0.2 lollipop in sabresd-imx6q board.

init: cannot expand '$ro.product.manufacturer' while writing to '/sys/class/android_usb/android0/iManufac'

init: using deprecated syntax for specifying property 'ro.product.model', use ${name} instead

init: property 'ro.product.model' doesn't exist while expanding '$ro.product.model'

init: cannot expand '$ro.product.model' while writing to '/sys/class/android_usb/android0/iProduct'

android_usb: already disabled

read descriptors

read strings

mtp_bind_config

binder: 147:147 transaction failed 29189, size 0-0

binder: 147:147 transaction failed 29189, size 0-0

binder: 147:147 transaction failed 29189, size 0-0

binder: 147:147 transaction failed 29189, size 0-0

binder: 147:147 transaction failed 29189, size 0-0

This binder: 147:147 transaction failed 29189, size 0-0 message keep on occur in my serial terminal but in sabresd board dispaly i didn't get anything...

help me to solve this one thanks in advance

0 Kudos
Reply

1,565 Views
wangtsungli
Contributor IV

Hi chandrasekharmattaparthy‌

I am getting the same issue too.

I get binder: 185:185 transaction failed 29189, size 0-0

Did you solve the problem yet?

0 Kudos
Reply