Problem running NXP TJA1100 with IMX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem running NXP TJA1100 with IMX6

2,493件の閲覧回数
mdmosaddekhossa
Contributor II

I have setup my device tree according to the specification of NXP TJA1100.


        pinctrl_enet: enetgrp { /* Ethernet MII */
            fsl,pins = <
                MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN         0x000130B0
                MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER          0x000130B0
                MX6QDL_PAD_KEY_COL0__ENET_RX_DATA3         0x000130B0
                MX6QDL_PAD_KEY_COL2__ENET_RX_DATA2         0x0001B0B0
                MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0        0x000130B0
                MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1        0x0001B0B0
                MX6QDL_PAD_ENET_MDC__ENET_MDC              0x000130B0
                MX6QDL_PAD_ENET_MDIO__ENET_MDIO            0x0001B0B0
                MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0        0x000130B0
                MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1        0x0001B0B0
                MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN          0x000130B0
                MX6QDL_PAD_KEY_ROW0__ENET_TX_DATA3         0x000130B0
                MX6QDL_PAD_KEY_ROW2__ENET_TX_DATA2         0x000130B0
                MX6QDL_PAD_GPIO_18__ENET_RX_CLK            0x0001B0B0
                MX6QDL_PAD_ENET_REF_CLK__ENET_TX_CLK       0x0001B0B0
                MX6QDL_PAD_KEY_COL4__GPIO4_IO14            0x000130B0
            >;
        };

/*Ethernet*/
&fec{
    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_enet>;
    phy-mode = "mii";
    phy-handle = <&ethphy>;
    phy-reset-gpios = <&gpio4 14 1>;  //todo
    status = "okay";  
   mdio {
        ethphy: ethernet-phy@06{
            compatible = "0x0180dc48";
            device_type = "ethernet-phy";
            reg = <0>;
        };
    };
};

First problem is it does not recognize other registers but only 0. When zero is assigned then it shows an error.

Error message: "fec 2188000.ethernet eth0: MDIO read timeout" and "TJA1100 2188000.ethernet:06: read error: did_interrupt failed"

Their is an link up error.  It will be really helpful for any suggestion as I am stuck with this problem for 3 weeks. I cannot find any solution.

0 件の賞賛
返信
2 返答(返信)

1,814件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi MD Mosaddek Hossain

one can look at  linux/drivers/net/phy/nxp

linux.git - Automotive Linux Tree 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,814件の閲覧回数
mdmosaddekhossa
Contributor II

I have already created a patch for this driver and I am running the driver according to the specification. But it does not recognize the phy address. 

0 件の賞賛
返信