Series Termination Resistor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Series Termination Resistor

2,075 次查看
johnnynguyen
Contributor I

I am connecting the i.MX6UL device with an FPGA through an RMII interface. Since this is a high speed transmission line which needs a series termination resistor. I assume maximum drive strength has typ impedance value is 23Ohm based on the datasheet, and it would need a 30Ohm resistor in series to die out the reflected voltage at load. Any recommendation for this topic?

标签 (1)
1 回复

1,860 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please look at some comments below regarding the issue.

 

1.

  Customers can refer to section 3.5.2 (High speed signal routing recommendations) of Hardware Development Guide for the i.MX 6UL.

 

https://www.nxp.com/docs/en/user-guide/IMX6ULHDG.pdf  

 

2.

  IMX 6UL EVK may be used as an example.

 

https://www.nxp.com/downloads/en/schematics/MCIMX6UL-EVK_DESIGNFILES.zip 

 

i.MX6UltraLite Evaluation Kit|NXP 

 

 

3.

  Customers can apply modeling, using IBIS files.

 

i.MX 6UltraLite Applications Processor|NXP 

 


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------