Problem libsdl2 on i.MX6DL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem libsdl2 on i.MX6DL

1,511件の閲覧回数
domenicoacri
Contributor III

Hello everyone,

i have a problem with the libsdl2 on the processor i.MX6DL.

I'm trying to render an image through these libraries and use hardware accelerators.

This does not seem to work, the only solution seems to be the use of software accelerators.

I'm using x11 and libraries libsdl2_2.0.5.

The libsdl2 are configuration with the following features :

--enable-video-opengl

--enable-video-x11

Best Regards

Domenico Acri

ラベル(4)
0 件の賞賛
返信
1 返信

1,172件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

refer to the other customer feedback, can support libsdl, not libsdl2, maybe you can try to use libsdl, and check if your local.conf include this.

0 件の賞賛
返信