Problem libsdl2 on i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem libsdl2 on i.MX6DL

1,512 Views
domenicoacri
Contributor III

Hello everyone,

i have a problem with the libsdl2 on the processor i.MX6DL.

I'm trying to render an image through these libraries and use hardware accelerators.

This does not seem to work, the only solution seems to be the use of software accelerators.

I'm using x11 and libraries libsdl2_2.0.5.

The libsdl2 are configuration with the following features :

--enable-video-opengl

--enable-video-x11

Best Regards

Domenico Acri

Labels (4)
0 Kudos
Reply
1 Reply

1,173 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the other customer feedback, can support libsdl, not libsdl2, maybe you can try to use libsdl, and check if your local.conf include this.

0 Kudos
Reply