Problem in Qt5 in MCIMX6UL-EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem in Qt5 in MCIMX6UL-EVK

1,006 Views
ko-hey
Senior Contributor II

Hi all

My customer is using following environment and have some problem.

So let me confirm about Qt5 support in MCIMX6UL-EVK.

・MCIMX6UL-EVK

     Branch : imx-3.14.38-6UL_ga, imx_4.1.15_1.0.0_ga

     Machine : imx6ulevk

     Backend : X11

     Project : fsl-image-qt5 

My customer want to try Qt5 app and touch the icon which is shown on the screen.

But it didn't response.

I think it caused i.MX6UL doesn't have GPU.

Is it correct ?

Ko-hey

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

832 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ko-hey,

Yes, you are right. There is no internal GPU on MCIMX6UL. If you need high Operational Capability on 3D, here I recommend you to use the other i.mx6 series products with GPU. Hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply