Question: how to compile the "device_program" in ATK R1.60 ?
Context: "i.MX Platform Advanced Tool Kit (ATK) Standard R1.60"
I'm working with a legacy product based on a i.MX27 board.
As I understand the ram kernel mx27_nand.bin
may be obtained from this ATK R1.60.
As the old gnu toolchain is not available anymore
(ref. doc. "ATK Reference Guide Standard Version.pdf")
I'm working with a recent toolchain for gnu arm.
I modified accordingly the file "rules.make":
------rules.make----------
CC = arm-none-eabi-gcc
AS = arm-none-eabi-as
LD = arm-none-eabi-ld
NM = arm-none-eabi-nm
OBJDUMP = arm-none-eabi-objdump
OBJCOPY = arm-none-eabi-objcopy
READELF = arm-none-eabi-readelf
RM = rm -f
RN = mv
CP = cp
TOPDIR = $(shell pwd)
BIN = arm-none-eabi-objcopy
LIBDIR = "/usr/lib/gcc/arm-none-eabi/5.2.1/"
SHELL = /bin/sh
CFLAGS = -Wall -Wstrict-prototypes -Wno-trigraphs -nostartfiles -O0 -nostdlib \
-static -feliminate-unused-debug-symbols -fno-strict-aliasing -fno-common \
-pipe -fno-builtin -g -mapcs -mlittle-endian \
-msoft-float -mfpu=vfp
------rules.make----------
where the modifs are for CC & other variables and the option -mfpu=vfp for the floating point unit.
When I try to compile with:
"make MCU=mx27 flashlib FLASH_TYPE=NAND"
I get the following errors:
-------
ram_kernel/ramkernel.o: In function `pop_usb_dqh':
device_program/ram_kernel/src/platform/mx27/channel.c:559: undefined reference to `memcpy'
ram_kernel/ramkernel.o: In function `push_usb_dqh':
device_program/ram_kernel/src/platform/mx27/channel.c:566: undefined reference to `memcpy'
flash/flashlib.o: In function `write_bbt':
device_program/flash/nand_flash/src/nand_bbt.c:553: undefined reference to `memset'
device_program/flash/nand_flash/src/nand_bbt.c:557: undefined reference to `memcpy'
flash/flashlib.o: In function `nand_update_bbt':
device_program/flash/nand_flash/src/nand_bbt.c:728: undefined reference to `malloc'
device_program/flash/nand_flash/src/nand_bbt.c:760: undefined reference to `free'
flash/flashlib.o: In function `nand_scan_bbt':
device_program/flash/nand_flash/src/nand_bbt.c:844: undefined reference to `malloc'
device_program/flash/nand_flash/src/nand_bbt.c:859: undefined reference to `free'
flash/flashlib.o: In function `nand_init':
device_program/flash/nand_flash/src/nand_flash.c:128: undefined reference to `malloc'
device_program/flash/nand_flash/src/nand_flash.c:130: undefined reference to `memset'
flash/flashlib.o: In function `nand_erase_conditional':
device_program/flash/nand_flash/src/nand_flash.c:428: undefined reference to `free'
flash/flashlib.o: In function `nand_write_page':
device_program/flash/nand_flash/src/nfc_base.c:360: undefined reference to `memset'
collect2: error: ld returned 1 exit status
-------
It seems like the ram kernel should link with the std libc, but on the compile flags
we have "-nostartfiles -nostdlib", hence not the std libs asked...
My question is: what am I missing as a library to link to this ram kernel ?
Hi Federico
one can look at more newer 1.71 ATK version
Programmers (Flash, etc.) (1)
Source Code for the Flash tool used for downloading, programing, dumping
and erasing images in Flash memory to the i.MX EVKs (REV 1.71)
regarding gcc errors one can post on gcc forum
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------