Problem halting iMX6 Chips (ARM Cortex-A9) at reset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem halting iMX6 Chips (ARM Cortex-A9) at reset

ソリューションへジャンプ
4,799件の閲覧回数
nathanpalmer
Contributor IV

Has anyone figured out how to halt the iMX6 (Cortex-A9) CPU just after or at reset?  My reset-init is taking too long to halt and I am ending up with a non-predictable system debug environment.  It loads the CPU boot ROM and is well into initializing my boot loader (U-Boot) before the halt takes affect.

In order to use OpenOCD I have to erase U-Boot from FLASH, and even then the ROM boot code is executed. 

I am hoping that some one here has a clue on making a more reliable iMX6 (actually an iMX6sl) debug environment.

Thanks!

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
4,001件の閲覧回数
leoschwab
Contributor III

Based on by disjointed readings on the subject, I think the semi-official method on the i.MX6 series is to force the device into serial bootloader mode (BOOT_MODE0 == 1, BOOT_MODE1 == 0), leaving the USB port unconnected.  When halt finally takes effect, the PC will be in the on-chip ROM waiting for a USB connection.  Change the PC to where you want and resume the CPU from there ('resume <address>').  At the very least, U-Boot won't have been loaded or run.

Please note that I have not had any actual success doing this myself, as I outlined here.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
4,002件の閲覧回数
leoschwab
Contributor III

Based on by disjointed readings on the subject, I think the semi-official method on the i.MX6 series is to force the device into serial bootloader mode (BOOT_MODE0 == 1, BOOT_MODE1 == 0), leaving the USB port unconnected.  When halt finally takes effect, the PC will be in the on-chip ROM waiting for a USB connection.  Change the PC to where you want and resume the CPU from there ('resume <address>').  At the very least, U-Boot won't have been loaded or run.

Please note that I have not had any actual success doing this myself, as I outlined here.

0 件の賞賛
返信
4,001件の閲覧回数
nathanpalmer
Contributor IV

That sucks for boards that don't have jumpers for that (production boards).  Is there a plan or at least a technical approach to support reset halts in OpenOCD for the MX6?  Sorry to ask OpenOCD questions here, I just suspect that the audience would have run across this issue before and may be tracking it.

0 件の賞賛
返信
4,001件の閲覧回数
Yuri
NXP Employee
NXP Employee

  The only i.MX35 of i.MX series has special so called startup mode :

"Upon reset the PC register will remain at address 0x00000000.
This means no ROM code has run so far and the state of all internal
SOC registers are untouched." 

  Perhaps, the fact, that it is impossible to stop the ARM core just
after reset relates to HAB technology - to avoid ROM code hacking.