Problem about imx28 GPMI NAND timing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem about imx28 GPMI NAND timing

1,607 Views
x10
Contributor V

Hi, All

I config imx28 GPMI NAND with following parameters:

   1. gpmi clock = 120MHz

   2. NandTiming.DataSetup = 40ns

   3. NandTiming.DataHold   = 30ns

   4. NandTiming.AddressSetup = 30ns

   5. RDN_DELAY = 0, DLL_ENABLE = 0

The above settings works fine with K9F1G08U0C, but get ECC error with K9F1G08U0D quite often. It's appreciated for any comments.

BR

Cheng Shi

emtronix

Labels (1)
0 Kudos
Reply
1 Reply

1,270 Views
x10
Contributor V

The nandflash RD# pin is set with 1.8V level in freeescale iMX28BSP of wince6.0, After setting to 3.3V level, all the ecc error were gone. The problem is fixed. 

BR

Cheng Shi

emtronix

0 Kudos
Reply