Hi,
I am not sure could I ask this question here?
I use the newest 3.10.17_GA Yocto bsp and try to bitbake the meta-toolchain-qte, but I got some errors.
Here is my command:
> MACHINE=imx6qsabresd source fsl-setup-release.sh –b build –e fb
> bitbake meta-toolchain-qte
Here is my error message:
user@user-N550JK:~/fsl-yocto/build$ bitbake meta-toolchain-qte
WARNING: Host distribution "Ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |###########################################| ETA: 00:00:00
Loaded 2005 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies
NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)
NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg
ERROR: Nothing PROVIDES 'nativesdk-libx11' (but /home/user/fsl-yocto/sources/poky/meta/recipes-qt/qt4/nativesdk-qt4-tools_4.8.5.bb DEPENDS on or otherwise requires it)
ERROR: nativesdk-libx11 was skipped: 'x11' not in DISTRO_FEATURES
NOTE: Runtime target 'nativesdk-qt4-tools' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['nativesdk-qt4-tools', 'nativesdk-libx11']
NOTE: Runtime target 'nativesdk-packagegroup-qte-toolchain-host' is unbuildable, removing...
Missing or unbuildable dependency chain was: ['nativesdk-packagegroup-qte-toolchain-host', 'nativesdk-qt4-tools', 'nativesdk-libx11']
ERROR: Required build target 'meta-toolchain-qte' has no buildable providers.
Missing or unbuildable dependency chain was: ['meta-toolchain-qte', 'nativesdk-packagegroup-qte-toolchain-host', 'nativesdk-qt4-tools', 'nativesdk-libx11']
Does anyone have any information about this?
BR
Brian
 
					
				
		
 alejandrolozan1
		
			alejandrolozan1
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
I am not sure if this should work on Ubuntu 14.04. I tried and followed the below training:
With Ubuntu 12.04 and it worked without any issue.
Can you try with that distribution?
Best Regards,
Alejandro
Hi,
I have temporarily found a solution.
The problem is due to the "DEPENDS" in the "nativesdk-qt4-tools.inc".
The "DEPENDS" in the inc file: DEPENDS = "nativesdk-zlib nativesdk-dbus nativesdk-libx11 qt4-native"
And I have the DISTRO_FEATURES_remove = "x11 wayland directfb "
So you will get the error message while you bitbake meta-toolchain-qte.
The temporary solution is just modify the "DEPENDS" in the "nativesdk-qt4-tools.inc" when you want to bitbake meta-toolchain-qte.
DEPENDS = "nativesdk-zlib nativesdk-dbus qt4-native"
BR
Brian