Problem about build the meta-toolchain-qte on newest release Yocto bsp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem about build the meta-toolchain-qte on newest release Yocto bsp

4,550件の閲覧回数
brianwu
Contributor III

Hi,

I am not sure could I ask this question here?

I use the newest 3.10.17_GA Yocto bsp and try to bitbake the meta-toolchain-qte, but I got some errors.

Here is my command:

> MACHINE=imx6qsabresd source fsl-setup-release.sh –b build –e fb

> bitbake meta-toolchain-qte

Here is my error message:

user@user-N550JK:~/fsl-yocto/build$ bitbake meta-toolchain-qte

WARNING: Host distribution "Ubuntu-14.04" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.

Loading cache: 100% |###########################################| ETA:  00:00:00

Loaded 2005 entries from dependency cache.

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

ERROR: Nothing PROVIDES 'nativesdk-libx11' (but /home/user/fsl-yocto/sources/poky/meta/recipes-qt/qt4/nativesdk-qt4-tools_4.8.5.bb DEPENDS on or otherwise requires it)

ERROR: nativesdk-libx11 was skipped: 'x11' not in DISTRO_FEATURES

NOTE: Runtime target 'nativesdk-qt4-tools' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['nativesdk-qt4-tools', 'nativesdk-libx11']

NOTE: Runtime target 'nativesdk-packagegroup-qte-toolchain-host' is unbuildable, removing...

Missing or unbuildable dependency chain was: ['nativesdk-packagegroup-qte-toolchain-host', 'nativesdk-qt4-tools', 'nativesdk-libx11']

ERROR: Required build target 'meta-toolchain-qte' has no buildable providers.

Missing or unbuildable dependency chain was: ['meta-toolchain-qte', 'nativesdk-packagegroup-qte-toolchain-host', 'nativesdk-qt4-tools', 'nativesdk-libx11']

Does anyone have any information about this?

BR

Brian

ラベル(2)
タグ(2)
3 返答(返信)

2,308件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

I am not sure if this should work on Ubuntu 14.04. I tried and followed the below training:

Yocto Training - HOME

With Ubuntu 12.04 and it worked without any issue.

Can you try with that distribution?

Best Regards,

Alejandro

0 件の賞賛
返信

2,308件の閲覧回数
brianwu
Contributor III

Hi,

I have temporarily found a solution.

The problem is due to the "DEPENDS" in the "nativesdk-qt4-tools.inc".

The "DEPENDS" in the inc file:  DEPENDS = "nativesdk-zlib nativesdk-dbus nativesdk-libx11 qt4-native"

And I have the DISTRO_FEATURES_remove = "x11 wayland directfb "

So you will get the error message while you bitbake meta-toolchain-qte.

The temporary solution is just modify the "DEPENDS" in the "nativesdk-qt4-tools.inc" when you want to bitbake meta-toolchain-qte.

DEPENDS = "nativesdk-zlib nativesdk-dbus qt4-native"

BR

Brian

2,308件の閲覧回数
olias
Contributor II

Thank you,

This is correct.  In my case though, it lead to another issue:

RDEPENDS_libgl-mx6-dev = "libgl-mesa-dev"

in gpu-viv-bin-mx6q.inc which I also removed.

0 件の賞賛
返信