Preempt-RT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Preempt-RT

Jump to solution
2,562 Views
ChrisChang1234
Contributor III

1. I'm looking for the patches that 'Only' enables the "Preemt-RT" feature.

    refer to 

    https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Enable-Linux-RT-PREEMPT-on-i-MX8M-Products/t...

But I don't know how get the patches for kernel 5.10.72 and 6.1.1x.

 

2.  Per customer's request, we have to replace the original rootfs with other version.

    If we do so, will the "Preempt RT" feature keep available?

    (in other words, the preempt rt patches impact kernel image only or also including the roots?) 

   

    

Labels (1)
0 Kudos
Reply
1 Solution
2,535 Views
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

View solution in original post

0 Kudos
Reply
2 Replies
2,527 Views
ChrisChang1234
Contributor III

Got it, thanks

0 Kudos
Reply
2,536 Views
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

0 Kudos
Reply