Preempt-RT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,602件の閲覧回数
ChrisChang1234
Contributor III

1. I'm looking for the patches that 'Only' enables the "Preemt-RT" feature.

    refer to 

    https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Enable-Linux-RT-PREEMPT-on-i-MX8M-Products/t...

But I don't know how get the patches for kernel 5.10.72 and 6.1.1x.

 

2.  Per customer's request, we have to replace the original rootfs with other version.

    If we do so, will the "Preempt RT" feature keep available?

    (in other words, the preempt rt patches impact kernel image only or also including the roots?) 

   

    

ラベル(1)
0 件の賞賛
返信
1 解決策
2,575件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,567件の閲覧回数
ChrisChang1234
Contributor III

Got it, thanks

0 件の賞賛
返信
2,576件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

1)the owner doesn't update to the latest bsp version, maybe customer needs to change the new bsp source code according to the patches based on 4.1478

2) refer to the readme, these patches are for kernel, customer just needs to change the kernel image, they just replace the new kernel image only

0 件の賞賛
返信