Power supply for eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power supply for eMMC

Jump to solution
3,058 Views
huydt1
Contributor II

Hi,

I'm design new device with imx7D saber as reference.

For reducing the extra LDO for suppling power to eMMC, I supply power eMMC by the LDO4 of PC32PF3000A1EP (LDO4: 3.3V, 350mA max, supply power to eMMC only)

Please help me check whether this modify is ok or not!

Thanks and best regards,

Dinh Huy 

Labels (2)
1 Solution
2,800 Views
igorpadykov
NXP Employee
NXP Employee

Hi DINH 

seems this will be fine, provided that processor power up sequence is

followed, 350mA should be sufficient for normal emmc operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
2,801 Views
igorpadykov
NXP Employee
NXP Employee

Hi DINH 

seems this will be fine, provided that processor power up sequence is

followed, 350mA should be sufficient for normal emmc operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,800 Views
huydt1
Contributor II

Thanks for your support

Dinh Huy

0 Kudos
Reply