Power supply for eMMC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power supply for eMMC

ソリューションへジャンプ
3,137件の閲覧回数
huydt1
Contributor II

Hi,

I'm design new device with imx7D saber as reference.

For reducing the extra LDO for suppling power to eMMC, I supply power eMMC by the LDO4 of PC32PF3000A1EP (LDO4: 3.3V, 350mA max, supply power to eMMC only)

Please help me check whether this modify is ok or not!

Thanks and best regards,

Dinh Huy 

ラベル(2)
1 解決策
2,879件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DINH 

seems this will be fine, provided that processor power up sequence is

followed, 350mA should be sufficient for normal emmc operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

2 返答(返信)
2,880件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi DINH 

seems this will be fine, provided that processor power up sequence is

followed, 350mA should be sufficient for normal emmc operation.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,879件の閲覧回数
huydt1
Contributor II

Thanks for your support

Dinh Huy

0 件の賞賛
返信