Power source of Secure JTAG (i.MX.RT1015)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power source of Secure JTAG (i.MX.RT1015)

跳至解决方案
1,107 次查看
Daehyeon
Contributor I

Hi,

I using a MIMXRT1015-EVK board.

In i.MX.RT1015, what is the power source of SJC(Secure JTAG Controller) component (especially, response comparison such as the following figure)?

(ex. DCDC_IN, SOC_IN, VDD_SNVS_IN, ...)

Daehyeon_0-1657026075537.png

 

标记 (2)
0 项奖励
回复
1 解答
1,099 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
SJC is on SOC so the power source is VDD_SOC_IN:

Omar_Anguiano_0-1657218776330.png

 

If you have more questions do not hesitate to ask me.
Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,100 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.
SJC is on SOC so the power source is VDD_SOC_IN:

Omar_Anguiano_0-1657218776330.png

 

If you have more questions do not hesitate to ask me.
Best regards,
Omar

0 项奖励
回复