Power input of VDDARM23_IN in i.MX6Dual.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power input of VDDARM23_IN in i.MX6Dual.

跳至解决方案
1,181 次查看
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

[Q1]

Refer to schematic of i.MX6Q SABRE-AI.

I'd like to use i.MX6Dual and VDDARM23_IN_x connect to ground.

Is it possible to remove these decoupling capacitors (C62, C613, C614, C615, C616, C617, C620) with i.MX 6Dual system?

[Q2]

If the voltage input to VDDARM23_IN_x on i.MX6Dual system, what problem is there?

(Increase the leak current? Destroy the CPU?)

Best Regards,

Keita

标签 (1)
0 项奖励
回复
1 解答
1,001 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes it is possible to remove these decoupling capacitors.

2. no problem, may be Increase of leak current.

Similar to that, i.MX6Solo/DualLite have one VDDARM_IN input

for both cores, Solo has one core disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,002 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes it is possible to remove these decoupling capacitors.

2. no problem, may be Increase of leak current.

Similar to that, i.MX6Solo/DualLite have one VDDARM_IN input

for both cores, Solo has one core disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复