Power input of VDDARM23_IN in i.MX6Dual.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power input of VDDARM23_IN in i.MX6Dual.

ソリューションへジャンプ
1,164件の閲覧回数
keitanagashima
Senior Contributor I

Dear Sir or Madam,

Hello.

[Q1]

Refer to schematic of i.MX6Q SABRE-AI.

I'd like to use i.MX6Dual and VDDARM23_IN_x connect to ground.

Is it possible to remove these decoupling capacitors (C62, C613, C614, C615, C616, C617, C620) with i.MX 6Dual system?

[Q2]

If the voltage input to VDDARM23_IN_x on i.MX6Dual system, what problem is there?

(Increase the leak current? Destroy the CPU?)

Best Regards,

Keita

ラベル(1)
0 件の賞賛
返信
1 解決策
984件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes it is possible to remove these decoupling capacitors.

2. no problem, may be Increase of leak current.

Similar to that, i.MX6Solo/DualLite have one VDDARM_IN input

for both cores, Solo has one core disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
985件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Keita

1. yes it is possible to remove these decoupling capacitors.

2. no problem, may be Increase of leak current.

Similar to that, i.MX6Solo/DualLite have one VDDARM_IN input

for both cores, Solo has one core disabled.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信