Porting HAB cst tool to non-Linux platforms?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting HAB cst tool to non-Linux platforms?

1,324 Views
mklug_xx
Contributor I

Is there any support to port the HAB signing tool to other platforms than Linux?

What are the conditions under which access to "the missing sources" is granted?

We might need the signing tool under Windows.

Regards

Mike

0 Kudos
Reply
1 Reply

1,072 Views
Yuri
NXP Employee
NXP Employee

Hello,

    You may look at Appendix B (Replacing the CST Backend Implementation)

of HAB CodeSigning Tool User’s Guide ("HABCST_UG.pdf') for CST implementation

details. As we can see only Linux is supported.

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 Kudos
Reply