Freescale DDR3 script not have the option for to set DDR3-1866 memory type

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Freescale DDR3 script not have the option for to set DDR3-1866 memory type

ソリューションへジャンプ
1,656件の閲覧回数
aravinthkumarja
Senior Contributor II

Hi all,

We are using micron DRAM (MT41K256M16) -DDR3-1866 memory type.

For this i need to configure in uboot .cfg file. So i use the below named excel file.

Mx6DQSDL DDR3 Script Aid V0.08.xlsx

But this excel script not have the option of DDR3-1866. So how can i configure this??

Any other updated script is there??

Recommend if anything other script available??

if any other procedure is there guide me??

Regards,

Aravinth

0 件の賞賛
返信
1 解決策
1,101件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency

is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for

533 MHz (1066).

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,102件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  i.MX6 supports DDR3/LVDDR3/LPDDR2-1066; maximum DRAM frequency

is 533 MHz. Therefore the "more speedy" DRAM parts, should be configured for

533 MHz (1066).

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信