Porting HAB cst tool to non-Linux platforms?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting HAB cst tool to non-Linux platforms?

1,840件の閲覧回数
mklug_xx
Contributor I

Is there any support to port the HAB signing tool to other platforms than Linux?

What are the conditions under which access to "the missing sources" is granted?

We might need the signing tool under Windows.

Regards

Mike

0 件の賞賛
返信
1 返信

1,588件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

    You may look at Appendix B (Replacing the CST Backend Implementation)

of HAB CodeSigning Tool User’s Guide ("HABCST_UG.pdf') for CST implementation

details. As we can see only Linux is supported.

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信