Porting a DP83869 driver to imx8qxp. My device tree for the phy is given below. It references imx8qxp.dtsi which references imx8-ss-conn.dtsi.
The eth0 on module phy is has an MDIO address of 5b040000.ethernet. The eth1 external custom phy using the DP83869 is assumed to have a MDIO address of 5b050000.ethernet inherited from imx8-ss-conn.dtsi.
fec1: ethernet@5b040000 {
reg = <0x5b040000 0x10000>;
interrupts = <GIC_SPI 258 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 256 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 257 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 259 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&enet0_lpcg 4>,
<&enet0_lpcg 2>,
<&enet0_lpcg 3>,
<&enet0_lpcg 0>,
<&enet0_lpcg 1>;
clock-names = "ipg", "ahb", "enet_clk_ref", "ptp", "enet_2x_txclk";
assigned-clocks = <&clk IMX_SC_R_ENET_0 IMX_SC_PM_CLK_PER>,
<&clk IMX_SC_R_ENET_0 IMX_SC_C_CLKDIV>;
assigned-clock-rates = <250000000>, <125000000>;
fsl,num-tx-queues=<3>;
fsl,num-rx-queues=<3>;
power-domains = <&pd IMX_SC_R_ENET_0>;
status = "disabled";
};
fec2: ethernet@5b050000 {
reg = <0x5b050000 0x10000>;
interrupts = <GIC_SPI 262 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 260 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 261 IRQ_TYPE_LEVEL_HIGH>,
<GIC_SPI 263 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&enet1_lpcg 4>,
<&enet1_lpcg 2>,
<&enet1_lpcg 3>,
<&enet1_lpcg 0>,
<&enet1_lpcg 1>;
clock-names = "ipg", "ahb", "enet_clk_ref", "ptp", "enet_2x_txclk";
assigned-clocks = <&clk IMX_SC_R_ENET_1 IMX_SC_PM_CLK_PER>,
<&clk IMX_SC_R_ENET_1 IMX_SC_C_CLKDIV>;
assigned-clock-rates = <250000000>, <125000000>;
fsl,num-tx-queues=<3>;
fsl,num-rx-queues=<3>;
power-domains = <&pd IMX_SC_R_ENET_1>;
status = "disabled";
};
My device tree has the following:
&fec2 {
//reg = <0x5b000000 0x10000>;
reg = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_fec2>;
compatible = "fsl,imx8qxp-fec", "fsl,imx8qm-fec";
fsl,magic-packet;
fsl,rgmii_rxc_dly;
fsl,rgmii_txc_dly;
phy-mode = "rgmii";
phy-handle = <ðphy1>;
enable-active-high;
regulator-always-on;
regulator-min-microvolt = <3300000>;
regulator-max-microvolt = <3300000>;
phy-reset-gpios = <&gpio_b 9 GPIO_ACTIVE_LOW>;
phy-reset-duration = <1000>;
status = "okay";
mdio {
#address-cells = <1>;
#size-cells = <0>;
status = "okay";
ethphy1: ethernet-phy@1 {
interrupt-parent = <&lsio_gpio3>;
interrupts = <18 IRQ_TYPE_LEVEL_LOW>;
micrel,led-mode = <0>;
rx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
tx-fifo-depth = <DP83869_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,op-mode = <DP83869_RGMII_COPPER_ETHERNET>;
ti,max-output-impedance = "true";
ti,clk-output-sel = <DP83869_CLK_O_SEL_REF_CLK>;
rx-internal-delay-ps = <2000>; /* 250 - 4000 in steps of 250 */
tx-internal-delay-ps = <2000>;
}
voltage regulator seems fine, 3.3V on phy enable and 1.8v on MDIO interface. Not seeing the correct MDIO address since device tree defaults to 5 and not address 0. 0 is the default address of the chip for the MDIO address. Also, the DP83869_RGMII_COPPER_ETHERNET op_mode is not being picked up by the driver.
1) How do I change the MDIO address to 0?
2) How do I pass the DP83869_RGMII_COPPER_ETHERNET property from this device tree to the driver?
I receive the message fec 5b050000.ethernet eth1: Unable to connect to phy. So, the MDIO address is not zero, it is defaulting to 5 instead?