Portable Scanner On iMX258

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Portable Scanner On iMX258

2,739 Views
vaibhavingale
Contributor I

I am working on iMX258 board which is used as ePOS. I would like to interface it with portable scanner, specifically Plustek S400.

Can someone please guide me how I can use this with POS? Do I need to write driver? I am using Linux Kernel Version 2.6 with QT support.

Labels (4)
Tags (3)
2 Replies

2,589 Views
SergioSolis
NXP Employee
NXP Employee

Hello Vaibhav,

Being that the scanner you are mentioning is USB, you can use the USB-HID driver in the linux BSP, the driver part would be covered with that.

2,589 Views
vaibhavingale
Contributor I

Thanks a lot for pointer, am working on it to make a tiny scanner application.

0 Kudos
Reply