Portable Scanner On iMX258

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Portable Scanner On iMX258

2,788件の閲覧回数
vaibhavingale
Contributor I

I am working on iMX258 board which is used as ePOS. I would like to interface it with portable scanner, specifically Plustek S400.

Can someone please guide me how I can use this with POS? Do I need to write driver? I am using Linux Kernel Version 2.6 with QT support.

ラベル(4)
タグ(3)
2 返答(返信)

2,638件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello Vaibhav,

Being that the scanner you are mentioning is USB, you can use the USB-HID driver in the linux BSP, the driver part would be covered with that.

2,638件の閲覧回数
vaibhavingale
Contributor I

Thanks a lot for pointer, am working on it to make a tiny scanner application.

0 件の賞賛
返信