Populate MIPI to enable?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Populate MIPI to enable?

ソリューションへジャンプ
2,487件の閲覧回数
JohnCannizzo
Contributor III

I have a Sabre board with iMX6Q, and I noticed the MIPI port (J5) is not populated. I looked at the current schematic, and it shows the MIPI components "not populated".  This seems like such an elementary question that has probably been asked many times, but I couldn't find it.  If I populate the MIPI components (J5, C602, C50, SH501, U10, R26, C585, C588, C28, C29, L10, L25, R726, C30, C587) will the MIPI port work from a hardware standpoint?  I plan on purchasing a MIPI camera for a surveillance / face recognition project, and want to insure it will interface to the Sabre.

Thanks...

John

ラベル(1)
0 件の賞賛
返信
1 解決策
2,359件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it should work, as schematic is similar to SDP board

SPF-27417 i.MX6_SABRE_SDP_DESIGNFILES

where MIPI port (J5) is populated.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,360件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi John

yes it should work, as schematic is similar to SDP board

SPF-27417 i.MX6_SABRE_SDP_DESIGNFILES

where MIPI port (J5) is populated.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,359件の閲覧回数
JohnCannizzo
Contributor III

Thanks, I'll order the parts...

0 件の賞賛
返信