Issue in Display bringup in imx6 sololite

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue in Display bringup in imx6 sololite

834 次查看
shrimanthramesh
Contributor I

We are porting 3.10 kernel for our custom board based on imx6sl.
In imx6sl.dtsi file, It is shown that driver is compatible with "fsl,imx28-lcdif", so we are enabling it to bringup the display.
when we enable "MXS LCD framebuffer support" to bringup the display, the kernel stops in between(Please see the below log)

Memory: 447MB 64MB = 511MB total
Memory: 243392k/243392k available, 280896k reserved, 0K highmem
Virtual kernel memory layout:
  vector : 0xffff0000 - 0xffff1000 ( 4 kB)
  fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
  vmalloc : 0xa0800000 - 0xff000000 (1512 MB)
  lowmem : 0x80000000 - 0xa0000000 ( 512 MB)
  pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
  modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
  .text : 0x80008000 - 0x809fa4b0 (10186 kB)
  .init : 0x809fb000 - 0x80a57600 ( 370 kB)
  .data : 0x80a58000 - 0x80a80ca0 ( 164 kB)
  .bss : 0x80affc44 - 0x80b8f9d0 ( 576 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
  RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
NR_IRQS:16 nr_irqs:16 16
L310 cache controller enabled
l2x0: 16 ways, CACHE_ID 0x410000c8, AUX_CTRL 0x32030000, Cache size: 262144 B


But when we disable the "Support for frame buffer devices" option in device drivers --> graphics, we are able to successfully boot the system.(without display)

We are using following:
bootargs:
setenv bootargs console=ttymxc2,115200 init=/init androidboot.console=ttymxc2 consoleblank=0 androidboot.hardware=freescale

dts:
imx6sl-evk-ldo.dts

Please let us know what we are missing. Thanks in advance

0 项奖励
回复
0 回复数