Player based on imX8MQ board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Player based on imX8MQ board

1,185件の閲覧回数
Joe_C
Contributor I

I used the yocto provided by the player in the routine, and copy it into the board, the path of the routine for "build - xwayland/TMP/work/aarch64 - poky - Linux/qtmultimedia 5.12.3 + gitAUTOINC + 64981 aee3b r0 / image/usr/share/examples/multimediawidgets/player".When playing A video, the CPU is 100% used, and the terminal prints out A Warning:A lot of buffers are being dropped.What can I do to play the video properly using this routineque1.png

0 件の賞賛
返信
3 返答(返信)

1,177件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

how about adding

IMAGE_INSTALL_append = "\
qtmultimedia \
qtmultimedia-plugins \
qtmultimedia-examples \
qtmultimedia-qmlplugins" to the local.conf,  and add PACKAGECONFIG_append_pn-qtmultimedia = " gstreamer" to local.conf too, then when the board boot up, to find /usr/share/examples/multimedia/video/qmlvideo

 

 

0 件の賞賛
返信

1,163件の閲覧回数
Joe_C
Contributor I

thanks,I have loaded the required modules into the system as you said. Based on this, I developed a player that can play videos normally, but if I frequently adjust the progress or volume of videos, the system will crash and restart.Please give me some instructions on how To solve this problem. 

0 件の賞賛
返信

1,082件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

current qt multimedia only supports play video normally, if you need other feature, customer needs debug by themselves, we don't offer these, or you can find more information from QT forum to further information

 

0 件の賞賛
返信