Picture display error in uboot

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Picture display error in uboot

1,801件の閲覧回数
jimmyli
Contributor IV

Chip: MIMX8MM6DVTLZAA

BSP:  L5.4.70-2.3.0, uboot version is 2020.04

Dispplay: mipi to RGB by LT9211, referent driver has been modified and initialized.

            Screen resolution: 1024*600referent configuration has been checked OK.

 

Question:

In uboot stage, the screen displays as below.

From uboot to kernel, kernel will read the same frame buffer transmitted from uboot,  the display is OK.

 

What is the reason for it, and how to fix ?

Thanks.

jimmyli_0-1624005608580.png

 

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,797件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Jimmy

 

for that issue one can recheck mipi clocks as described on :

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-i-MX8M-Mini-and-Nano-MIPI-DPHY-C...

 

Best regards
igor

0 件の賞賛
返信

1,786件の閲覧回数
jimmyli
Contributor IV

Hi Igor,

      We will check again.

      Thanks.

0 件の賞賛
返信

1,771件の閲覧回数
mesahin
Contributor I

Hello jimmyli,

Can you share  reference driver LT9211 ?

Sincerely.

0 件の賞賛
返信