Picture display error in uboot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Picture display error in uboot

1,828 次查看
jimmyli
Contributor IV

Chip: MIMX8MM6DVTLZAA

BSP:  L5.4.70-2.3.0, uboot version is 2020.04

Dispplay: mipi to RGB by LT9211, referent driver has been modified and initialized.

            Screen resolution: 1024*600referent configuration has been checked OK.

 

Question:

In uboot stage, the screen displays as below.

From uboot to kernel, kernel will read the same frame buffer transmitted from uboot,  the display is OK.

 

What is the reason for it, and how to fix ?

Thanks.

jimmyli_0-1624005608580.png

 

标签 (1)
0 项奖励
回复
3 回复数

1,824 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jimmy

 

for that issue one can recheck mipi clocks as described on :

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-i-MX8M-Mini-and-Nano-MIPI-DPHY-C...

 

Best regards
igor

0 项奖励
回复

1,813 次查看
jimmyli
Contributor IV

Hi Igor,

      We will check again.

      Thanks.

0 项奖励
回复

1,798 次查看
mesahin
Contributor I

Hello jimmyli,

Can you share  reference driver LT9211 ?

Sincerely.

0 项奖励
回复