Patched CVEs database

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Patched CVEs database

2,285 Views
habib_farahani
Contributor III

Hello,

 

Recently, I upgraded the kernel on our i.MX6UL based board to 5.10.120.  As I was going through CVE database in NVD, I realized some patches were already applied by NXP.  Is there an internal database that maintains a list of applied patches by NXP so that I can focus only by the unapplied patches?

 

Thanks you in advance

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

2,284 Views
habib_farahani
Contributor III

Incidentally, I have visited https://cve.report/vendor/nxp however, some of the patches that are already applied are not listed.

0 Kudos
Reply

2,264 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello 

The CVE need to pass an strictly selection is probably that your patch simple not pass, you need to be a CNA, however is you want you can add our patches to https://www.cve.org/ResourcesSupport/Resources

Regards

 

0 Kudos
Reply

2,250 Views
habib_farahani
Contributor III

Hi,

 

Thanks for your reply!  I think you misunderstood my question.  I was wondering if NXP has implemented patches for any CVEs against Linix_kernel 5.10.120.  If so, please share the CVE records with me .  Not necessarily the patches.

 

Best,

Habib Farahani

0 Kudos
Reply