Parameters for imx8mp HDMI pixel clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Parameters for imx8mp HDMI pixel clock

Jump to solution
2,321 Views
TeroLP
Contributor I

linux-imx has samsung_phy_pll_cfg defined in drivers/phy/freescale/phy-fsl-samsung-hdmi.c . To support HDMI display with certain pixel clock, config struct has to have parameters for that frequency.

I'm using evalutation kit, and would need parameters for two clocks:
238760000 (2560x1440) and 150000000 (1920x1200).

I would appreciate a ready made table or a tool to generate that table.

0 Kudos
Reply
1 Solution
2,310 Views
joanxie
NXP TechSupport
NXP TechSupport

I've mailed to you, pls check it

View solution in original post

0 Kudos
Reply
5 Replies
2,311 Views
joanxie
NXP TechSupport
NXP TechSupport

I've mailed to you, pls check it

0 Kudos
Reply
1,715 Views
Miles_x
Contributor I

Hi, joanxie

I have a simliar problem,  use iMX8MP platform, HDMI 1280x800@60HZ output,  please send me the tool, thanks!

0 Kudos
Reply
1,711 Views
joanxie
NXP TechSupport
NXP TechSupport

this isn't available for customers, pls create a new case for your display, and tell me what pixel clock you need

 

0 Kudos
Reply
1,693 Views
Miles_x
Contributor I
0 Kudos
Reply
2,169 Views
Stefano_Radaelli
Contributor I

Hello,

can I have those informations please? I have to add a 2560x1440 HDMI display, with 241500000
 clock. Is it possible?

Thank you,

Stefano

0 Kudos
Reply