Panel can't display correct Android screen

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Panel can't display correct Android screen

930 次查看
bensonhuang
Contributor III

Hi,

We are using i.MX8M for our development platform.

Panel is 800x480 resolution (7 inch).

We use Yocto Linux and Android to test if the panel can display the screen.

For Yocto Linux (fsl-yocto-L4.9.51_mx8mq-ga), the panel can display correct screen of x-wayland.

For Android (imx-o8.0.0_1.3.0_8mq-prc), we can't show the correct screen.

The attached files are the frame buffer shown on Vyson and the screen shown on the panel.

Could you please help to give us some advice how to solve the issue?

Thanks.

S__27508753.jpg

S__27508752.jpg

标签 (4)
0 项奖励
回复
1 回复

810 次查看
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please tell me the display that you are using? 

Best Regards,

Diego

0 项奖励
回复