Panel can't display correct Android screen

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Panel can't display correct Android screen

1,349 Views
bensonhuang
Contributor III

Hi,

We are using i.MX8M for our development platform.

Panel is 800x480 resolution (7 inch).

We use Yocto Linux and Android to test if the panel can display the screen.

For Yocto Linux (fsl-yocto-L4.9.51_mx8mq-ga), the panel can display correct screen of x-wayland.

For Android (imx-o8.0.0_1.3.0_8mq-prc), we can't show the correct screen.

The attached files are the frame buffer shown on Vyson and the screen shown on the panel.

Could you please help to give us some advice how to solve the issue?

Thanks.

S__27508753.jpg

S__27508752.jpg

Labels (4)
0 Kudos
Reply
1 Reply

1,229 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Can you please tell me the display that you are using? 

Best Regards,

Diego

0 Kudos
Reply