Package manager issue in imx6ull board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Package manager issue in imx6ull board

860 次查看
Et_MM
Contributor II

Hi,

I am working on a custom board based on imx6ull evk. I am facing issues regarding package manager.  i am not able to install any package using apt.
when i checked the distribution package repository it was empty.

root@imx6ul7d:~# cat /etc/apt/sources.list

root@imx6ul7d:~# ls /etc/apt/sources.list.d/
root@imx6ul7d:~#

root@imx6ul7d:~# cat /etc/os-release
ID=fsl-imx-xwayland
NAME="NXP i.MX Release Distro"
VERSION="6.6-scarthgap (scarthgap)"
VERSION_ID=6.6-scarthgap
VERSION_CODENAME="scarthgap"
PRETTY_NAME="NXP i.MX Release Distro 6.6-scarthgap (scarthgap)"
CPE_NAME="cpe:/o:openembedded:fsl-imx-xwayland:6.6-scarthgap"
root@imx6ul7d:~#

please walk me through the procedure to resolve the packet manager issue.

0 项奖励
回复
3 回复数

795 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Our BSP only provides the package manager apt. Unfortunately, we do not provide the enhanced security certification requirements since the Debian 10 repo. It is recommended to add packages using Yocto build, or other tools such as dpkg.

 

Regards

Harvey

0 项奖励
回复

793 次查看
Et_MM
Contributor II

Thanks for the reply and I will try this.

So,this means there are no package managers that can be installed or used with the i.MX6ULL?

0 项奖励
回复

775 次查看
Harvey021
NXP TechSupport
NXP TechSupport

Regarding this security certification requirement, so far, I think so.

 

Regards

Harvey

0 项奖励
回复