Package manager issue in imx6ull board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Package manager issue in imx6ull board

1,008件の閲覧回数
Et_MM
Contributor II

Hi,

I am working on a custom board based on imx6ull evk. I am facing issues regarding package manager.  i am not able to install any package using apt.
when i checked the distribution package repository it was empty.

root@imx6ul7d:~# cat /etc/apt/sources.list

root@imx6ul7d:~# ls /etc/apt/sources.list.d/
root@imx6ul7d:~#

root@imx6ul7d:~# cat /etc/os-release
ID=fsl-imx-xwayland
NAME="NXP i.MX Release Distro"
VERSION="6.6-scarthgap (scarthgap)"
VERSION_ID=6.6-scarthgap
VERSION_CODENAME="scarthgap"
PRETTY_NAME="NXP i.MX Release Distro 6.6-scarthgap (scarthgap)"
CPE_NAME="cpe:/o:openembedded:fsl-imx-xwayland:6.6-scarthgap"
root@imx6ul7d:~#

please walk me through the procedure to resolve the packet manager issue.

0 件の賞賛
返信
3 返答(返信)

943件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Our BSP only provides the package manager apt. Unfortunately, we do not provide the enhanced security certification requirements since the Debian 10 repo. It is recommended to add packages using Yocto build, or other tools such as dpkg.

 

Regards

Harvey

0 件の賞賛
返信

941件の閲覧回数
Et_MM
Contributor II

Thanks for the reply and I will try this.

So,this means there are no package managers that can be installed or used with the i.MX6ULL?

0 件の賞賛
返信

923件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Regarding this security certification requirement, so far, I think so.

 

Regards

Harvey

0 件の賞賛
返信