PXP testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PXP testing

4,948件の閲覧回数
EricNelson
Senior Contributor II

Hi all,

We've had an ongoing discussion on the meta-freescale list about how to test the Pixel Pipeline (PXP) device.
     https://lists.yoctoproject.org/pipermail/meta-freescale/2015-April/thread.html#13349

In short, it appears that the unit_test program for the PXP is broken and not well documented, though the
gstreamer-1.0 pxp elements are partially functional.

Carlos used the gstreamer elements to perform a very thorough test of all pixel formats that are advertised by the driver:

     https://lists.yoctoproject.org/pipermail/meta-freescale/2015-April/013376.html

It appears that support for many are broken.

Please join the conversation if you have knowledge in this area.

4 返答(返信)

3,316件の閲覧回数
LaurenPost
NXP Employee
NXP Employee

I did forward the community thread on and waiting for a reply from the team that owns PXP.

PXP (includdng unit test cases) will have updates in next release but not sure if that addresses this issue you reported.

3,316件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

I tested PXP unit-test with the latest imx7D release and I faced exactly the same error.

0 件の賞賛
返信

3,316件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

OtavioSalvador, can you please comment on this?

0 件の賞賛
返信

3,316件の閲覧回数
EricNelson
Senior Contributor II

Hi James,

Otavio is the one who pointed out that we weren't including PXP in our device tree!

0 件の賞賛
返信