Hi everyone,
I'm working on a custom board which uses a TLV320AIC3105 Audio Codec connected to an i.MX6.
I already managed to get Linux 3.14 and Debian 8 running with it.
The Linux Kernel is from here:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/snapshot/rel_imx_3.14.28_1.0.0_ga.tar.gz
Debian is installed by debootstrap as described here:
https://community.freescale.com/docs/DOC-95044#comment-27229
My next step after the GUI (KDE) is to get some sound out of the machine. And now I have a weird Problem:
The driver I need for this codec isn't available in the kernel's menuconfig. I have searched for it and got following result:
Symbol: SND_SOC_TLV320AIC3X [=n]
Type : tristate
Defined at sound/soc/codecs/Kconfig:380
Depends on: SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y]
Selected by: SND_DAVINCI_SOC_GENERIC_EVM [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y]
|| SND_OMAP_SOC_N810 [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y] && SND_OMAP_SOC [=n] && MACH_NOKIA_N810 [=n] && I2C [=y] && OMAP_MUX [=n]
|| SND_OMAP_SOC_RX51 [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y] && SND_OMAP_SOC [=n] && ARM [=y] && (MACH_NOKIA_RX51 [=n]
|| COMPILE_TEST [=n]) && GPIOLIB [=y]
|| SND_SOC_SAMSUNG_SIMTEC_HERMES [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y] && SND_SOC_SAMSUNG [=n] && ARCH_S3C24XX [=n]
|| SND_S6000_SOC_S6IPCAM [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y] && SND_S6000_SOC [=n] && XTENSA_PLATFORM_S6105
|| SND_SOC_ALL_CODECS [=n] && SOUND [=y] && !M68K && !UML && SND [=y] && SND_SOC [=y] && COMPILE_TEST [=n] && I2C [=y]
This gives me the answer, that the driver will not be compiled and the option isn't available, because there is no Path to this option.
In my opinion, the dependencies are OK. So why is the Driver not available?
I also merged the mentioned Kconfig with the corresponding Kconfig of Kernel 3.19. After this merge, the Driver was available. But the compiled Kernel boots straight into an Oops with a NULL-Pointer-Exception.
Manually add the entry "CONFIG_SND_SOC_TLV320AIC3X=y" to the .config without the merge doesn't work. The driver will not be compiled and the entry is gone after compilation.
The Codec is connected to I2C3. Here's my device tree:
i2c3: i2c@021a8000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
reg = <0x021a8000 0x4000>;
interrupts = <0 38 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_I2C3>;
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c3>;
status = "okay";
tlv320aic3105: tlv320aic3105@18 {
compatible = "ti,tlv320aic3x";
reg = <0x18>;
};
};
The Codec is also shown in the Output of "i2cdetect -y 2" with address 0x18.
Any Ideas how to solve this?
Thanks for the fast answer, but:
You need to enable driver in
sound/soc/codec
- The driver TLV320AIC3X(.c) is in this folder, OK. But it is NOT available in the kernel menuconfig. So I can not enable it. Why is this driver not available?
The whole Codec-Driver menu is not available!
Platform specific code in
sound/soc/fsl
- In the Platform specific code ther is an "Eukrea TLV320". Is this Compatible with TI TLV320AIC3105? I don't think so, but if yes, what is the compatible string?
For more detail check attached document
Chapter 8
Porting Audio Codecs to a Custom Board
This chapter is far to short to answer all of my questions:
- I need three nodes in my device tree: ssi, codec and sound. Correct?
- The "codec" is the I2C-connection in my first post, right?
- We don't supply the codec by imx, we supply it by on-board power sources. So the AVDD, DCVDD etc. entries are not nessesary?
The only connections between imx and the codec is I2C and I2S.
- There is no "fsl-*-tlv320aic3x" compatible string (therefore there is no such driver or vice versa). Do I have to write something by my own, or can I use something like "simple-audio-card"?
Hi
Steffen
You need to modify following files to add support for your driver.
You can refer WM8962 and make change accordingly.
sound/soc/codecs/Kconfig
sound/soc/codecs/Makefile
sound/soc/fsl/Kconfig
sound/soc/fsl/Makefile
Thanks
Saurabh
I tried this patch:
[PATCH 2/5] ASoC: fsl: add imx-tlv320aic3x machine driver
It should make the tlv320aic3x driver available by accomodating
sound/soc/fsl/Kconfig and sound/soc/fsl/Makefile
it doesn't change something in
sound/soc/codecs/Kconfig and sound/soc/codecs/Makefile
Also it adds the imx-tlv320aicx.c driver and some documentation.
Then I editet my devicetree like this:
sound {
compatible = "fsl,imx-audio-tlv320aic3x";
model = "imx6q-phyflex-tlv320aic3007";
ssi-controller = <&ssi2>;
audio-codec = <&tlv320aic3105>;
audio-routing =
"Line Out", "LLOUT",
"Line Out", "RLOUT",
"Headphone Jack", "HPLOUT",
"Headphone Jack", "HPROUT";
};
ssi2: ssi@0202c000 {
compatible = "fsl,imx6q-ssi","fsl,imx21-ssi";
reg = <0x0202c000 0x4000>;
interrupts = <0 47 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_SSI2_IPG>,
<&clks IMX6QDL_CLK_SSI2>;
clock-names = "ipg", "baud";
dmas = <&sdma 41 1 0>,
<&sdma 42 1 0>;
dma-names = "rx", "tx";
fsl,fifo-depth = <15>;
fsl,ssi-dma-events = <42 41>;
fsl,mode = "i2s-slave";
status = "okay";
};
/* I2C to Touch, Audio, Camera */
i2c3: i2c@021a8000 {
#address-cells = <1>;
#size-cells = <0>;
compatible = "fsl,imx6q-i2c", "fsl,imx21-i2c";
reg = <0x021a8000 0x4000>;
interrupts = <0 38 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_I2C3>;
clock-frequency = <100000>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c3>;
status = "okay";
tlv320aic3105: tlv320aic3105@18 {
compatible = "ti,tlv320aic310x", "ti,tlv320aic3x";
reg = <0x18>;
clocks = <&clks 201>;
};
};
And this is what I get after compilation and start of the kernel:
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
ci_hdrc ci_hdrc.1: EHCI Host Controller
ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
hub 2-0:1.0: USB hub found
hub 2-0:1.0: 1 port detected
mousedev: PS/2 mouse device common for all mice
input: EP0810M09 as /devices/soc0/soc.8/2100000.aips-bus/21a8000.i2c/i2c-2/2-0038/input/input0
snvs_rtc 20cc034.snvs-rtc-lp: rtc core: registered 20cc034.snvs-rtc-lp as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR RC5 (streamzap) protocol handler initialized
IR SANYO protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
mxc_v4l2_output v4l2_out.24: V4L2 device registered as video16
mxc_v4l2_output v4l2_out.24: V4L2 device registered as video17
lm75 0-0048: hwmon0: sensor 'lm75'
lm75 1-0048: hwmon1: sensor 'lm75'
i2c-core: driver [mag3110] using legacy suspend method
i2c-core: driver [mag3110] using legacy resume method
0-001c supply vdd not found, using dummy regulator
0-001c supply vddio not found, using dummy regulator
input: mma845x as /devices/virtual/input/input1
imx2-wdt 20bc000.wdog: IMX2+ Watchdog Timer enabled. timeout=60s (nowayout=0)
Bluetooth: HCI UART driver ver 2.2
Bluetooth: HCI H4 protocol initialized
Bluetooth: HCI BCSP protocol initialized
Bluetooth: HCIATH3K protocol initialized
usbcore: registered new interface driver bcm203x
usbcore: registered new interface driver btusb
Bluetooth: Generic Bluetooth SDIO driver ver 0.1
usbcore: registered new interface driver ath3k
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
sdhci-esdhc-imx 2190000.usdhc: could not get ultra high speed state, work on normal mode
mmc0: no vqmmc regulator found
usb 1-1: new high-speed USB device number 2 using ci_hdrc
mmc0: no vmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata1.00: ATA-7: SFCA32GBH1BR4TO-I-NC-236-STD, 20111021, max UDMA/133
ata1.00: 62586880 sectors, multi 0: LBA48
ata1.00: configured for UDMA/133
scsi 0:0:0:0: Direct-Access ATA SFCA32GBH1BR4TO- 1021 PQ: 0 ANSI: 5
sd 0:0:0:0: [sda] 62586880 512-byte logical blocks: (32.0 GB/29.8 GiB)
sd 0:0:0:0: [sda] Write Protect is off
sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA
sdhci-esdhc-imx 2198000.usdhc: could not get ultra high speed state, work on normal mode
sda: sda1
sd 0:0:0:0: [sda] Attached SCSI disk
mmc2: no vqmmc regulator found
mmc2: no vmmc regulator found
mmc0: new high speed SDHC card at address 59b4
mmcblk0: mmc0:59b4 SDC 29.4 GiB
mmcblk0: p1 p2 p3
mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
mmc3: no vqmmc regulator found
mmc3: no vmmc regulator found
hub 1-1:1.0: USB hub found
hub 1-1:1.0: 4 ports detected
mmc3: SDHCI controller on 219c000.usdhc [219c000.usdhc] using ADMA
/soc/aips-bus@02000000/vpu@02040000: could not get #power-domain-cells for /soc/aips-bus@02000000/gpc@020dc000
mxc_vpu 2040000.vpu: VPU initialized
Job Ring Device allocation for transform failed
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
Unable to handle kernel NULL pointer dereference at virtual address 00000014
pgd = 80004000
[00000014] *pgd=00000000
Internal error: Oops: 5 [#1] PREEMPT SMP ARM
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.14.28 #113
task: a8080000 ti: a8062000 task.ti: a8062000
PC is at aic3x_i2c_probe+0x84/0x310
LR is at _raw_spin_unlock_irqrestore+0x28/0x54
pc : [<805e97d0>] lr : [<8077fc6c>] psr: a0000113
sp : a8063e48 ip : a8063e14 fp : 00000000
r10: ab7508cc r9 : a8062000 r8 : 00000000
r7 : 00000000 r6 : a81af420 r5 : a840a910 r4 : a83aee50
r3 : 00000000 r2 : 00000000 r1 : a0000113 r0 : ffffffff
Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
Control: 10c53c7d Table: 1000404a DAC: 00000015
Process swapper/0 (pid: 1, stack limit = 0xa8062238)
Stack: (0xa8063e48 to 0xa8064000)
3e40: 00000000 a81af420 80ea5ecc a81af420 80ea5ecc a81af400
3e60: 80ea5ecc 00000000 80dfc510 804dfa3c a81af420 80f111ac 00000000 803dc3d0
3e80: a81af420 80ea5ecc a81af454 00000000 80e31cc4 803dc584 00000000 80ea5ecc
3ea0: 803dc4f8 803daba0 a80d4a5c a8199934 80ea5ecc a840ea00 80e8f4d8 803dbb60
3ec0: 80d6e5a8 80ea5ecc 00000006 80ea5ecc 00000006 80e416f8 80eb6f00 803dcba4
3ee0: 80e8f4d8 80ea5ea8 00000006 804e1810 00000000 80e4d3e0 00000006 800088a8
3f00: 80efcaa4 a810c100 807840c4 0000009f 80eb6f00 80dbd520 00000000 8012201c
3f20: 00000000 80e64b10 abfff9d8 807a6c48 00000118 80044ee4 80e64b04 80e4cb18
3f40: 80d492b4 80dbc3a0 00000006 00000006 80e64ae0 80e4d3e0 00000006 80e416f8
3f60: 80eb6f00 00000118 80e41704 80dfc510 00000000 80dfcbf8 00000006 00000006
3f80: 80dfc510 8004dc2c 00000000 807720bc 00000000 00000000 00000000 00000000
3fa0: 00000000 807720c4 00000000 8000e5b8 00000000 00000000 00000000 00000000
3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 44322cc0 0f9a83c8
[<805e97d0>] (aic3x_i2c_probe) from [<804dfa3c>] (i2c_device_probe+0x80/0xa8)
[<804dfa3c>] (i2c_device_probe) from [<803dc3d0>] (driver_probe_device+0x114/0x23c)
[<803dc3d0>] (driver_probe_device) from [<803dc584>] (__driver_attach+0x8c/0x90)
[<803dc584>] (__driver_attach) from [<803daba0>] (bus_for_each_dev+0x54/0x88)
[<803daba0>] (bus_for_each_dev) from [<803dbb60>] (bus_add_driver+0xd4/0x1d0)
[<803dbb60>] (bus_add_driver) from [<803dcba4>] (driver_register+0x78/0xf4)
[<803dcba4>] (driver_register) from [<804e1810>] (i2c_register_driver+0x2c/0xb4)
[<804e1810>] (i2c_register_driver) from [<800088a8>] (do_one_initcall+0xe4/0x140)
[<800088a8>] (do_one_initcall) from [<80dfcbf8>] (kernel_init_freeable+0xfc/0x1c8)
[<80dfcbf8>] (kernel_init_freeable) from [<807720c4>] (kernel_init+0x8/0xec)
[<807720c4>] (kernel_init) from [<8000e5b8>] (ret_from_fork+0x14/0x3c)
Code: e5973004 e5843078 e5973008 e5843098 (e5983014)
---[ end trace 22ed2c2097f97d93 ]---
Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
CPU2: stopping
CPU: 2 PID: 0 Comm: swapper/2 Tainted: G D 3.14.28 #113
[<800155a0>] (unwind_backtrace) from [<800116bc>] (show_stack+0x10/0x14)
[<800116bc>] (show_stack) from [<8077909c>] (dump_stack+0x6c/0xb8)
[<8077909c>] (dump_stack) from [<8001455c>] (handle_IPI+0x130/0x15c)
[<8001455c>] (handle_IPI) from [<800085a0>] (gic_handle_irq+0x54/0x5c)
[<800085a0>] (gic_handle_irq) from [<80012180>] (__irq_svc+0x40/0x70)
Exception stack(0xa80a9fa0 to 0xa80a9fe8)
9fa0: ffffffed 2a8e5000 80e5b374 8001d4c0 a80a8000 80e5a574 807835cc 80eb6c91
9fc0: 00000001 412fc09a 80eb6c91 00000000 00000000 a80a9fe8 8000f15c 8000f14c
9fe0: 60000113 ffffffff
[<80012180>] (__irq_svc) from [<8000f14c>] (arch_cpu_idle+0x28/0x44)
[<8000f14c>] (arch_cpu_idle) from [<80064ff4>] (cpu_startup_entry+0x5c/0x148)
[<80064ff4>] (cpu_startup_entry) from [<10008644>] (0x10008644)
CPU1: stopping
CPU: 1 PID: 0 Comm: swapper/1 Tainted: G D 3.14.28 #113
[<800155a0>] (unwind_backtrace) from [<800116bc>] (show_stack+0x10/0x14)
[<800116bc>] (show_stack) from [<8077909c>] (dump_stack+0x6c/0xb8)
[<8077909c>] (dump_stack) from [<8001455c>] (handle_IPI+0x130/0x15c)
[<8001455c>] (handle_IPI) from [<800085a0>] (gic_handle_irq+0x54/0x5c)
[<800085a0>] (gic_handle_irq) from [<80012180>] (__irq_svc+0x40/0x70)
Exception stack(0xa80a7fa0 to 0xa80a7fe8)
7fa0: ffffffed 2a8dd000 80e5b374 8001d4c0 a80a6000 80e5a574 807835cc 80eb6c91
7fc0: 00000001 412fc09a 80eb6c91 00000000 00000000 a80a7fe8 8000f15c 8000f14c
7fe0: 60000113 ffffffff
[<80012180>] (__irq_svc) from [<8000f14c>] (arch_cpu_idle+0x28/0x44)
[<8000f14c>] (arch_cpu_idle) from [<80064ff4>] (cpu_startup_entry+0x5c/0x148)
[<80064ff4>] (cpu_startup_entry) from [<10008644>] (0x10008644)
CPU3: stopping
CPU: 3 PID: 0 Comm: swapper/3 Tainted: G D 3.14.28 #113
[<800155a0>] (unwind_backtrace) from [<800116bc>] (show_stack+0x10/0x14)
[<800116bc>] (show_stack) from [<8077909c>] (dump_stack+0x6c/0xb8)
[<8077909c>] (dump_stack) from [<8001455c>] (handle_IPI+0x130/0x15c)
[<8001455c>] (handle_IPI) from [<800085a0>] (gic_handle_irq+0x54/0x5c)
[<800085a0>] (gic_handle_irq) from [<80012180>] (__irq_svc+0x40/0x70)
Exception stack(0xa80abfa0 to 0xa80abfe8)
bfa0: ffffffed 2a8ed000 80e5b374 8001d4c0 a80aa000 80e5a574 807835cc 80eb6c91
bfc0: 00000001 412fc09a 80eb6c91 00000000 00000000 a80abfe8 8000f15c 8000f14c
bfe0: 60000113 ffffffff
[<80012180>] (__irq_svc) from [<8000f14c>] (arch_cpu_idle+0x28/0x44)
[<8000f14c>] (arch_cpu_idle) from [<80064ff4>] (cpu_startup_entry+0x5c/0x148)
[<80064ff4>] (cpu_startup_entry) from [<10008644>] (0x10008644)
------------[ cut here ]------------
WARNING: CPU: 0 PID: 1 at kernel/workqueue.c:829 wq_worker_waking_up+0x68/0x80()
Modules linked in:
CPU: 0 PID: 1 Comm: swapper/0 Tainted: G D 3.14.28 #113
[<800155a0>] (unwind_backtrace) from [<800116bc>] (show_stack+0x10/0x14)
[<800116bc>] (show_stack) from [<8077909c>] (dump_stack+0x6c/0xb8)
[<8077909c>] (dump_stack) from [<8002ced0>] (warn_slowpath_common+0x64/0x88)
[<8002ced0>] (warn_slowpath_common) from [<8002cf10>] (warn_slowpath_null+0x1c/0x24)
[<8002cf10>] (warn_slowpath_null) from [<80041a30>] (wq_worker_waking_up+0x68/0x80)
[<80041a30>] (wq_worker_waking_up) from [<8004ed24>] (ttwu_do_activate.constprop.72+0x4c/0x60)
[<8004ed24>] (ttwu_do_activate.constprop.72) from [<80051890>] (try_to_wake_up+0x1b4/0x298)
[<80051890>] (try_to_wake_up) from [<8005d840>] (__wake_up_common+0x4c/0x80)
[<8005d840>] (__wake_up_common) from [<8005d888>] (__wake_up_locked+0x14/0x1c)
[<8005d888>] (__wake_up_locked) from [<8005dfbc>] (complete+0x34/0x44)
[<8005dfbc>] (complete) from [<804a649c>] (__usb_hcd_giveback_urb+0x5c/0xd4)
[<804a649c>] (__usb_hcd_giveback_urb) from [<804a659c>] (usb_giveback_urb_bh+0x88/0xc4)
[<804a659c>] (usb_giveback_urb_bh) from [<80031154>] (tasklet_action+0x64/0xf4)
[<80031154>] (tasklet_action) from [<80030924>] (__do_softirq+0xf4/0x204)
[<80030924>] (__do_softirq) from [<80030c9c>] (irq_exit+0xa8/0xec)
[<80030c9c>] (irq_exit) from [<8000ee04>] (handle_IRQ+0x3c/0x94)
[<8000ee04>] (handle_IRQ) from [<80008574>] (gic_handle_irq+0x28/0x5c)
[<80008574>] (gic_handle_irq) from [<80012180>] (__irq_svc+0x40/0x70)
Exception stack(0xa8063b90 to 0xa8063bd8)
3b80: 00000001 00000000 80ebbdfc 00000000
3ba0: 80eb89f0 80ce6774 a8080000 00000000 00000000 a8080000 805e97d2 805e97d4
3bc0: 000008d8 a8063bd8 8077fc6c 80774a10 60000113 ffffffff
[<80012180>] (__irq_svc) from [<80774a10>] (panic+0x14c/0x1bc)
[<80774a10>] (panic) from [<8002f104>] (do_exit+0x7e8/0x884)
[<8002f104>] (do_exit) from [<800118b8>] (die+0x1f8/0x3c0)
[<800118b8>] (die) from [<807748a4>] (__do_kernel_fault.part.9+0x54/0x74)
[<807748a4>] (__do_kernel_fault.part.9) from [<8001a194>] (do_page_fault+0x1a4/0x378)
[<8001a194>] (do_page_fault) from [<800083b4>] (do_DataAbort+0x34/0x98)
[<800083b4>] (do_DataAbort) from [<80012118>] (__dabt_svc+0x38/0x60)
Exception stack(0xa8063e00 to 0xa8063e48)
3e00: ffffffff a0000113 00000000 00000000 a83aee50 a840a910 a81af420 00000000
3e20: 00000000 a8062000 ab7508cc 00000000 a8063e14 a8063e48 8077fc6c 805e97d0
3e40: a0000113 ffffffff
[<80012118>] (__dabt_svc) from [<805e97d0>] (aic3x_i2c_probe+0x84/0x310)
[<805e97d0>] (aic3x_i2c_probe) from [<804dfa3c>] (i2c_device_probe+0x80/0xa8)
[<804dfa3c>] (i2c_device_probe) from [<803dc3d0>] (driver_probe_device+0x114/0x23c)
[<803dc3d0>] (driver_probe_device) from [<803dc584>] (__driver_attach+0x8c/0x90)
[<803dc584>] (__driver_attach) from [<803daba0>] (bus_for_each_dev+0x54/0x88)
[<803daba0>] (bus_for_each_dev) from [<803dbb60>] (bus_add_driver+0xd4/0x1d0)
[<803dbb60>] (bus_add_driver) from [<803dcba4>] (driver_register+0x78/0xf4)
[<803dcba4>] (driver_register) from [<804e1810>] (i2c_register_driver+0x2c/0xb4)
[<804e1810>] (i2c_register_driver) from [<800088a8>] (do_one_initcall+0xe4/0x140)
[<800088a8>] (do_one_initcall) from [<80dfcbf8>] (kernel_init_freeable+0xfc/0x1c8)
[<80dfcbf8>] (kernel_init_freeable) from [<807720c4>] (kernel_init+0x8/0xec)
[<807720c4>] (kernel_init) from [<8000e5b8>] (ret_from_fork+0x14/0x3c)
---[ end trace 22ed2c2097f97d94 ]---
Please Help, I'm not good In kernel debugging. (In fact I really have no clue!)
What does that mean?