PRELU compilation error on iMX8MP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PRELU compilation error on iMX8MP

Jump to solution
3,124 Views
jetxeberria
Contributor III

Hi,

I'm having issues compiling my model with PReLU activation for iMX8MP. This operation is supposed to be supported.

I'm converting and quantizing (to int8) the model from keras to tflite using quantization aware training with native tflite methods

k_model = keras.models.load_model(path_keras)
print("Converting Keras model to int8 tflite format")
converter = tf.lite.TFLiteConverter.from_keras_model(k_model)
converter.target_spec.supported_ops = [
tf.lite.OpsSet.TFLITE_BUILTINS,
tf.lite.OpsSet.TFLITE_BUILTINS_INT8,
]
converter.optimizations = [tf.lite.Optimize.DEFAULT]
converter.representative_dataset = tf.lite.RepresentativeDataset(
ImageDataset(shuffle=True, limit=200, channel_first=False, input_name="input_1").generator
)
converter.target_spec.supported_ops = [tf.lite.OpsSet.TFLITE_BUILTINS_INT8]
converter.inference_input_type = tf.int8
converter.inference_output_type = tf.int8
tflite_model = converter.convert()
with open(path_tflite, "wb") as f:
f.write(tflite_model)

This is the error:

Vx delegate: allowed_cache_mode set to 0.
Vx delegate: device num set to 0.
Vx delegate: allowed_builtin_code set to 0.
Vx delegate: error_during_init set to 0.
Vx delegate: error_during_prepare set to 0.
Vx delegate: error_during_invoke set to 0.
input: serving_default_input_1:0shape: [ 1 112 112 3] dtype: <class 'numpy.int8'>
W [HandleLayoutInfer:274]Op 162: default layout inference pass.
(267:0) : error : Error(0,267) : Cannot find the header file cl_viv_vx_ext.h.
(25:0) : error : undefined identifier: 'COPY'
(59:0) : error : undefined identifier: 'COPY'
(270:0) : error : syntax error at 'VXC_512Bits'

ERROR: Failed to compile vx shader. (error: FFFFFFFF)
E [kernel/vsi_nn_kernel.c:_gpu_register:600]Build program fail.
E [kernel/vsi_nn_kernel.c:vsi_nn_kernel_create_node:874]Register client kernel com.vivantecorp.extension.evis.prelu_U8U8toU8_2D fail with -1.
(267:0) : error : Error(0,267) : Cannot find the header file cl_viv_vx_ext.h.
(25:0) : error : undefined identifier: 'COPY'
(59:0) : error : undefined identifier: 'COPY'
(270:0) : error : syntax error at 'VXC_512Bits'

This is repeated for 49 times and then this last error is shown:

ERROR: Failed to compile vx shader. (error: FFFFFFFF)
E [kernel/vsi_nn_kernel.c:_gpu_register:600]Build program fail.
E [kernel/vsi_nn_kernel.c:vsi_nn_kernel_create_node:874]Register client kernel com.vivantecorp.extension.evis.prelu_U8U8toU8_2D fail with -1.

Do you identify this error? PReLU is supposed to work, why am I seeing this error?

Thanks in advance

 

1 Solution
2,992 Views
JeFi
Contributor II

I had an similar error this week. For me it was the missing header file cl_viv_vx_ext.h that is also missing in the error message. I think it was in the opencl recipe and the header file is only copied on the yocto image if something happens (its been too long), but what you can try: just create the header file with

https://github.com/larrylart/codrive/blob/master/hw_sampling/vim3_npu/include/aml_sdk/CL/cl_viv_vx_e...

and place it in the folder of youre executable.

Best wishes

View solution in original post

5 Replies
2,993 Views
JeFi
Contributor II

I had an similar error this week. For me it was the missing header file cl_viv_vx_ext.h that is also missing in the error message. I think it was in the opencl recipe and the header file is only copied on the yocto image if something happens (its been too long), but what you can try: just create the header file with

https://github.com/larrylart/codrive/blob/master/hw_sampling/vim3_npu/include/aml_sdk/CL/cl_viv_vx_e...

and place it in the folder of youre executable.

Best wishes

2,971 Views
jorgemf
Contributor I

This worked. Thanks!

Tags (1)
0 Kudos
Reply
3,001 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello.

 

Does this happens on 6.6.3v BSP? since is the first one that support PRELU.

Regards

0 Kudos
Reply
2,994 Views
jetxeberria
Contributor III

Hello Bio_TICFSL,

Thanks for your response.

We're using Kirkstone 5.15.71_2.2.0. Docs say it's supported: https://github.com/nxp-imx/tflite-vx-delegate-imx/blob/lf-5.15.71_2.2.0/op_status.md

0 Kudos
Reply
2,998 Views
jorgemf
Contributor I

it should be supported, at least it is state int he docs: https://github.com/nxp-imx/tflite-vx-delegate-imx/blob/lf-5.15.5_1.0.0/op_status.md

0 Kudos
Reply