PRE in devicetree

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PRE in devicetree

1,416 次查看
jotes
Contributor IV

Hello,

 

I would like to connect 2 PREs to one IPU (as shown in the diagram below). I am using fb0 and fb1 (overlay). As I understand, the both framebuffers can be connected to separate PRE. Could you please guide me how to add a proper entry in devicetree?

pastedImage_3.png

When I write:

&mxcfb1 { /* fb0 and fb1 */

            prefetch;

};

only the fb0 is using PRE.

 

Regards!

0 项奖励
回复
2 回复数

1,210 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi jotes,

Kernel config:

 

CONFIG_MXC_IPU_V3_PRE=y

CONFIG_MXC_IPU_V3_PRG=y

 

DTS File:

 

memory: memory {

reg = <0x10000000 0xefffffff>;

};

 

&mxcfb1 {

prefetch;

};

 

&pre1 {

status = "okay";

};

 

&pre2 {

status = "okay";

};

 

 

&prg1 {

memory-region = <&memory>;

status = "okay";

};

 

&prg2 {

memory-region = <&memory>;

status = "okay";

};

There is one PRG per IPU and each PRG can handshake between 1 to 3 PRE and one IPU. Please see the image below:

config_supported.png

 

PRE-0 is dedicated to IPU-1, PRE-3 is dedicated to IPU-2, PRE-1 and PRE-2 can be configured to be used together with either IPU-1 or IPU-2.

Regards

0 项奖励
回复

1,210 次查看
jotes
Contributor IV

Hello

Thanks for your answer, but is it possible to configure the devicetree to use 2 PRE for one display? Or should I modify the driver?

Regards

0 项奖励
回复