PPTP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PPTP

6,093件の閲覧回数
alexandrglukhov
Contributor III

Hello, I need your help in next problem:

I have an i.mx28 and a Linux on it. I'm using buildroot.

I want to connect to server, using pptp-linux client.

In buildroot I choose the pptp-linux client and pppd and do make. Then on i.mx28 I try to connect to server

pptp 92.x.x.x

Couldn't open the /dev/ppp device: No such device or address

/usr/sbin/pppd: Please load the ppp_generic kernel module.

ls -al /dev/ppp

crwxrwxrwx    1 root     root      108,   0 Nov 26  2014 /dev/ppp


I can't understand what should I do with it. Can you help me?

ラベル(2)
タグ(4)
0 件の賞賛
返信
3 返答(返信)

4,375件の閲覧回数
b36401
NXP Employee
NXP Employee

As pptp client requires PPP daemon you need to add ppp component as well with the BSP.
Also you can refer instructions for installing PPTP client Yury suggested:

http://pptpclient.sourceforge.net/howto-debian.phtml

0 件の賞賛
返信

4,375件の閲覧回数
alexandrglukhov
Contributor III

I already select pppd in buildroot. But I haven't got directories such as ets/ppp/peers or scripts like pon or poff. I tried to add them manually, but the error is the same:

Couldn't open the /dev/ppp device: No such device or address

/usr/sbin/pppd: Please load the ppp_generic kernel module.

0 件の賞賛
返信

4,375件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please check kernel configuration :

Device Drivers  --->

Network device support  --->

<*>   PPP (point-to-point protocol) support│

~Yuri.

0 件の賞賛
返信