POR_B Design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,752件の閲覧回数
Sam_ECU
Contributor V

Hello,

On the EVK for 1011 and 1062, the POR_B signal is pulled up to DCDC_3V3:

Sam_ECU_0-1708005288522.png

Sam_ECU_1-1708005343809.png

But then in AN13202, it's recommended to pull up the signal to SNVS:

https://www.nxp.com/docs/en/application-note/AN13202.pdf

Sam_ECU_2-1708005407484.png

Question:

What is the best voltage source or it doesn't matter?

 

Regards,

Sam

0 件の賞賛
返信
1 解決策
1,705件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sam_ECU,

The best practice for POR_B is to pull up to VDD_SNVS_IN, as mentioned on AN13202 as well as the Hardware Development Guide of each i.MX RT.

BR,
Edwin.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,706件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sam_ECU,

The best practice for POR_B is to pull up to VDD_SNVS_IN, as mentioned on AN13202 as well as the Hardware Development Guide of each i.MX RT.

BR,
Edwin.

0 件の賞賛
返信