PMIC on evaluation boards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC on evaluation boards

5,508 Views
JCP
Contributor I

Somebody knows why evaluation boards use a DA9053 PMIC instead of freescale MC13892 PMIC? Are there any problem with the MC13892 for this design?

 

Dialog don't have publish information about the DA9053 in the web. Also I don't find technical information, manuals, detail distributors or prices for this chip.

 

Thanks

Labels (1)
0 Kudos
Reply
8 Replies

5,016 Views
c10ud
Contributor I

Hello,

i'm not a "company" so i cannot request the DA9053 datasheet. I need to investigate on why the PMIC isn't powering the processor's RTC in my IMX53QSBs. No response from Freescale so far, i just wanted to see if there's any register in the DA9053 that controls that voltage and must be programmed with some value from uboot.

 

Ideas?

 

greets  

0 Kudos
Reply

5,016 Views
JessBrown
Contributor I

Hi, just thought I'd let you all know that there is a PMIC from Wolfson that supports the i.MX53. There are some designs in production using the WM8325 and the i.MX53.

http://www.wolfsonmicro.com/products/power_management/WM8325/

0 Kudos
Reply

5,016 Views
MarianoGoluboff
Contributor III

Oh yeah, I guess a link to the LTC3589 datasheet would be helpful:

http://cds.linear.com/docs/Datasheet/3589fc.pdf

0 Kudos
Reply

5,016 Views
TureNielsen
Contributor I

Dialog have now added a link so its possible to request a data sheet for the DA9053.

http://www.dialog-semiconductor.com/register_da9053.php

0 Kudos
Reply

5,016 Views
MarianoGoluboff
Contributor III

Take a look at Linear Technologies LTC3589-1. The i.MX53 System Development User's Guide has an example of how to use this PMIC with the i.MX53.

 

See section 5.3 of that document. You can download it here:

http://cache.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf?fpsp=1

0 Kudos
Reply

5,016 Views
iafg
Contributor III

The 13892 can't meet the current spec requirements.

Freescale will have a PMIC of their own to support this processor in the near future.

0 Kudos
Reply

5,016 Views
FelixVidal
Contributor I

Perhaps the MC34708FS is the ideal and final candidate to sustitute the MC13892 as PMIC on MX53 designs ?.

The only downside is that it is still under development and Freescale doesn't let us download a preliminary datasheet.

That's a pity.
0 Kudos
Reply

5,016 Views
MXLuser
Contributor I
I think the 13892 doesn't have the right default voltages and sequencing for the MX53. The 9053 is a better part for the job. You have to get the datasheet direct from them. http://www.dialog-semiconductor.com/
0 Kudos
Reply