Windows CE 7 BSP for imx53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Windows CE 7 BSP for imx53

3,408件の閲覧回数
seetha
Contributor III
Hi, I am working on imx53 board from freescale. I am a newbie to this world. Please help in getting Wince 7 BSP for imx53.
タグ(1)
0 件の賞賛
返信
4 返答(返信)

2,496件の閲覧回数
seetha
Contributor III

Hi Marsha ,

I am working on MCIMX53SMD and thanks a lot for your reply....

I got the BSP and I am building it.Everything is working fine except that touch controller.Does anybody know the reason for it.It is too slow in opening the icons on which I click.


Marsha Chang said:

Hello Seetharam, 

Which i.MX53 board are you working on?  

 

MCIMX53-START or MCIMX53SMD? Andrew's post is for the MCIMX53SMD.

Adeneo has the i.MX53 Quick Start board (MCIMX53-START) BSP available on their website.

http://www.adeneo-embedded.com/iMX53

0 件の賞賛
返信

2,496件の閲覧回数
marshachang
NXP Employee
NXP Employee

Hello Seetharam, 

Which i.MX53 board are you working on?  

 

MCIMX53-START or MCIMX53SMD? Andrew's post is for the MCIMX53SMD.

Adeneo has the i.MX53 Quick Start board (MCIMX53-START) BSP available on their website.

http://www.adeneo-embedded.com/iMX53

0 件の賞賛
返信

2,496件の閲覧回数
seetha
Contributor III

Thanks a lot Andrew...



Andrew I said:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIM...

Run-time Software (26)Expand All
Sort by Modified Date
Board Support Packages (14)
ID and Description Vendor Availability
IMX53_WCE700_1105_BSP_SOURCE : Windows Embedded Compact 7 BSP for i.MX53 Processor. Support SABRE Platform for Tablets and Automotive.
Size (K): 25551 Format: zip Rev #: 11.05 Modified: 6/23/2011 FREESCALE
Download
0 件の賞賛
返信

2,496件の閲覧回数
fear_nada
Contributor I
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=WEIMX&fpsp=1&tab=Design_Tools_Tab Run-time Software (26)Expand All Sort by Modified Date Board Support Packages (14) ID and Description Vendor Availability IMX53_WCE700_1105_BSP_SOURCE : Windows Embedded Compact 7 BSP for i.MX53 Processor. Support SABRE Platform for Tablets and Automotive. Size (K): 25551 Format: zip Rev #: 11.05 Modified: 6/23/2011 FREESCALE Download
0 件の賞賛
返信