PMIC SWBSTFB Max Rating

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC SWBSTFB Max Rating

Jump to solution
1,963 Views
danielkubiak
Contributor I

Hello,

The SWBSTFB max rating voltage is only 4.8V in the PF0100 data sheet (page 9).

It's a little bit surprising as the boost output voltage can go up to 5,15V.

Labels (1)
0 Kudos
Reply
1 Solution
1,859 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

View solution in original post

0 Kudos
Reply
2 Replies
1,860 Views
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

0 Kudos
Reply
1,859 Views
danielkubiak
Contributor I

Hi Jorge,

Thank you for your answer.

Best Regards

Daniel

0 Kudos
Reply