PMIC SWBSTFB Max Rating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC SWBSTFB Max Rating

ソリューションへジャンプ
1,964件の閲覧回数
danielkubiak
Contributor I

Hello,

The SWBSTFB max rating voltage is only 4.8V in the PF0100 data sheet (page 9).

It's a little bit surprising as the boost output voltage can go up to 5,15V.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,860件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,861件の閲覧回数
JorgeRama_rezRi
NXP Employee
NXP Employee

Hi Daniel,

This error has already been detected. The correct value is 5.5V. This is being corrected in the next rev of the datasheet, which should be released in the next couple of weeks.

Best regards.

Jorge.

0 件の賞賛
返信
1,860件の閲覧回数
danielkubiak
Contributor I

Hi Jorge,

Thank you for your answer.

Best Regards

Daniel

0 件の賞賛
返信