PMIC PF3000 minimum input for VSNVS on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC PF3000 minimum input for VSNVS on

Jump to solution
1,957 Views
frankyhsu
Contributor III

Hi

We are checking the PMIC minimum vin and we found when we set Vin=2.8V, the VSNVS output will be off. We have checked the PF3000 EVB and got the same symptom. In the datasheet, the minimum Vin should be 2.25V. Why is the VSNVS turned off @Vin=2.8V? 

pastedImage_1.png

Labels (2)
0 Kudos
Reply
1 Solution
1,735 Views
igorpadykov
NXP Employee
NXP Employee

Hi Franky

VSNVS output derives its power from either VIN using LDO, or coin cell.

LDO is used wnen VIN > VTH1 as described in sect.6.3.11 VSNVS LDO/switch,

Table 67. SNVS modes of operation, VTH1=2.75V (typ.), Table 16. Dynamic electrical

characteristics - VSNVS PF3000 Datasheet
https://www.nxp.com/docs/en/data-sheet/PF3000.pdf 

When powered by coin cell, the VSNVS output tracks the coin cell voltage by means of a switch.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,736 Views
igorpadykov
NXP Employee
NXP Employee

Hi Franky

VSNVS output derives its power from either VIN using LDO, or coin cell.

LDO is used wnen VIN > VTH1 as described in sect.6.3.11 VSNVS LDO/switch,

Table 67. SNVS modes of operation, VTH1=2.75V (typ.), Table 16. Dynamic electrical

characteristics - VSNVS PF3000 Datasheet
https://www.nxp.com/docs/en/data-sheet/PF3000.pdf 

When powered by coin cell, the VSNVS output tracks the coin cell voltage by means of a switch.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply